cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Discovery - ST-LINK

Legacy member
Not applicable
Posted on October 19, 2014 at 23:20

Hello,

I'm having issue to connect to my newly bought STM32F4 discovery board with the

- STM32 ST-LINK Utility v3.4.0

- StlinkUSB Driver V4.3.3.0

When I try to connect it's always failing with any parameter in the settings box.

https://sites.google.com/site/levequejerome/_/rsrc/1413753212515/home/version.jpg

https://sites.google.com/site/levequejerome/home/connect1.jpg?attredirects=0

https://sites.google.com/site/levequejerome/home/connect2.jpg?attredirects=0

Can you help me?

Kind regards

#st-link/v2-stm32f4discovery
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on October 20, 2014 at 03:45

Consider trying different USB cables, USB ports, or computer?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Legacy member
Not applicable
Posted on October 20, 2014 at 21:10

Hello,

Yes I did my laptop on Windows 8.1 64bits and Linux Debian 64bits desktop with 

https://github.com/texane/stlink

.

It looks with st-link that core_id is read as 0x00, if that's help anyone. 

Regards

Posted on October 21, 2014 at 01:40

Yeah, I'm not sure what to suggest, you could double check the jumpers connecting the ST-LINK SWD/SWCLK to the F4, and the 3V supply, and the voltage on the VCAP pins (1.25V).

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Legacy member
Not applicable
Posted on October 21, 2014 at 21:13

Hello Clive,

Thanks for trying to help me.

I've check today at my office with an oscilloscope and I've found the issue.

The signal T_JTCK is ok on the CN2 connector on both side of the resistor R12, but completely null on both side of the SB3. So on PIN 1 of the CN3 connector there is just a null signal.

The conclusion is the PA14 Pin of the STM32F4 does not receive a correct clock.

Conclusion ST-LINK does not work.

I will contact the seller for the warranty.

Kind regards

Jérôme