Skip to main content
shyam
Associate
March 20, 2017
Question

STM32f042 CAN Tx issue

  • March 20, 2017
  • 1 reply
  • 775 views
Posted on March 20, 2017 at 14:05

‌

https://community.st.com/tags♯/?tags=stm32%20can

‌

https://community.st.com/tags♯/?tags=can%20init

‌

https://community.st.com/tags♯/?tags=can%20bus

‌

https://community.st.com/tags♯/?tags=can%20code

‌

Hi,

      I am trying out CAN communication with STM32F042 Nucleo dev board. I am getting passive error all the time on Tx message. When i try to debug found last_error as passive and Tx_message status as pending. I dint think there is problem in the CAN initialization, my code is attached below. I am out of my thinking. I would be thankful if i can get some suggestions on this.

int main(void)

{

CanTxMsg TxMessage;

CanRxMsg RxMessage;

static unsigned int TxMailBox=0, Status =0, ErrStatus=0, RxErrCnt=0;

/*!< At this stage the microcontroller clock setting is already configured,

this is done through SystemInit() function which is called from startup

file (startup_stm32f0xx.s) before to branch to application main.

To reconfigure the default setting of SystemInit() function, refer to

system_stm32f0xx.c file

*/

RCC_init(); //Clock Setting

if (SysTick_Config(SystemCoreClock / 1000))

{

/* Capture error */

while (1);

}

/* CAN configuration */

CAN_Bus_Initialization();

/* Infinite loop */

while(1)

{

// CAN_SetSpeed(25 );

if(TickCont > 1000)

{

TickCont=0;

TxMessage.IDE = CAN_ID_STD;

TxMessage.StdId = 0x07;

TxMessage.ExtId = 0x00;

TxMessage.RTR = CAN_RTR_DATA;

TxMessage.DLC = 1;

TxMessage.Data[0] = 5;

if(TxMailBox != 4)

{

TxMailBox = CAN_Transmit(CANx, &TxMessage);

}

Status=CAN_TransmitStatus(CANx,TxMailBox);

// RxMessage.IDE = 0x00;

// RxMessage.StdId = CAN_ID_STD;

// RxMessage.ExtId = 0x00;

// RxMessage.RTR = CAN_RTR_DATA;

// RxMessage.DLC = 0;

// RxMessage.Data[0] = 0;

// CAN_Receive(CANx, CAN_FIFO0, &RxMessage);

ErrStatus=CAN_GetLastErrorCode(CAN);

// RxErrCnt = CAN_GetReceiveErrorCounter(CAN);

if(((CANx->ESR) & (uint8_t)CAN_ESR_EPVF))

{

ErrStatus |= CAN_ESR_EPVF;

}

else

{

ErrStatus &= ~CAN_ESR_EPVF;

}

if(((CANx->ESR) & (uint8_t)CAN_ESR_BOFF))

{

ErrStatus |= CAN_ESR_BOFF;

}

else

{

ErrStatus &= ~CAN_ESR_BOFF;

}

// Status=CAN_TransmitStatus(CANx,CAN_Transmit(CANx, &TxMessage));

// TxErrCnt = CAN_GetLSBTransmitErrorCounter(CAN);

}

}

}

//CanTxMsg TxMessage = {0};

void CAN_Bus_Initialization()

{

RCC->APB2ENR |= RCC_APB2ENR_SYSCFGCOMPEN;

SYSCFG->CFGR1 |= SYSCFG_CFGR1_PA11_PA12_RMP;

CAN_Config();

}

/**

* @brief Configures the CAN.

* @param None

* @retval None

*/

static void CAN_Config(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

NVIC_InitTypeDef NVIC_InitStructure;

CAN_InitTypeDef CAN_InitStructure;

CAN_FilterInitTypeDef CAN_FilterInitStructure;

/* CAN GPIOs configuration **************************************************/

/* Enable GPIO clock */

RCC_AHBPeriphClockCmd(CAN_GPIO_CLK, ENABLE);

/* Connect CAN pins to AF7 */

GPIO_PinAFConfig(CAN_GPIO_PORT, CAN1_RX_PIN_Source, CAN_AF_PORT );

GPIO_PinAFConfig(CAN_GPIO_PORT, CAN1_TX_PIN_Source, CAN_AF_PORT);

/* Configure CAN RX and TX pins */

GPIO_InitStructure.GPIO_Pin = CAN_RX_PIN | CAN_TX_PIN ;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

GPIO_Init(CAN_GPIO_PORT, &GPIO_InitStructure);

/* NVIC configuration *******************************************************/

// NVIC_InitStructure.NVIC_IRQChannel = CEC_CAN_IRQn;

// NVIC_InitStructure.NVIC_IRQChannelPriority = 3;

// NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

// NVIC_Init(&NVIC_InitStructure);

/* CAN configuration ********************************************************/

/* Enable CAN clock */

RCC_APB1PeriphClockCmd(CAN_CLK, ENABLE);

/* CAN register init */

CAN_DeInit(CANx);

CAN_StructInit(&CAN_InitStructure);

/* CAN cell init */

CAN_InitStructure.CAN_TTCM = DISABLE;

CAN_InitStructure.CAN_ABOM = ENABLE;

CAN_InitStructure.CAN_AWUM = DISABLE;

CAN_InitStructure.CAN_NART = DISABLE;

CAN_InitStructure.CAN_RFLM = DISABLE;

CAN_InitStructure.CAN_TXFP = DISABLE;

CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;

CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;

/* CAN Baudrate = 1MBps (CAN clocked at 48 MHz) */

&sharpif 1 // Sample-Pint : 50%

CAN_InitStructure.CAN_BS1 = CAN_BS1_9tq;

CAN_InitStructure.CAN_BS2 = CAN_BS2_8tq;

CAN_InitStructure.CAN_Prescaler = 2;

&sharpelse // Sample-Pint : 87.5%

CAN_InitStructure.CAN_BS1 = CAN_BS1_13tq;

CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq;// ErrStatus=CAN_GetLastErrorCode(CAN);

CAN_InitStructure.CAN_Prescaler = 12;

&sharpendif

CAN_Init(CANx, &CAN_InitStructure);

/* CAN filter init */

CAN_FilterInitStructure.CAN_FilterNumber = 0;

CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;

CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;

CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;

CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;

CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;

CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;

CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;

CAN_FilterInit(&CAN_FilterInitStructure);

// /* CAN FIFO0 message pending interrupt enable */

// CAN_ITConfig(CANx, CAN_IT_FMP0, ENABLE);

/* Enable FIFO 0 message pending Interrupt */

// CAN_ITConfig(CANx, CAN_IT_FMP0, ENABLE);

}

in regards,

Sundar.

#stm32-can #can-code #stm32f042can #stm32f042-swd #can-init #can-bus
This topic has been closed for replies.

1 reply

shyam
shyamAuthor
Associate
March 21, 2017
Posted on March 21, 2017 at 08:14

Error which i was getting is Form error and i debugged in scope to check the message, found some extra bits getting added to frame. 

thanks in advance.