Skip to main content
marcogrossi89
Associate III
April 12, 2018
Question

STM32F334R8T6 can not read memory

  • April 12, 2018
  • 0 replies
  • 759 views
Posted on April 12, 2018 at 10:08

I have designed a board with STM32F334R8T6. The STM32 pins are configured as in the attached file (I do not think there is a problem here since I have already used the same configuration without problems). The microcontroller is programmed with a STM32 NUCLEO BOARD using the 6-pins connector (3.3V, PA14, GND, PA13, NRST, PB3): also in this case I do not think there is a problem since I can program without problems other boards using the same NUCLEO board and connector.

When I try to connect to the STM32F334 microcontroller using STM32 ST-LINK utility I get the following message:

09:33:

03

: ST-LINK SN : 066BFF515056805087143648

09:33:

03

: ST-LINK Firmware version : V2J21M5

09:33:

03

: Connected via SWD.

09:33:

03

: Connection mode : Connect Under Reset.

09:33:

03

: Debug in Low Power mode enabled.

09:33:

04

: Device ID:0x438

09:33:

04

: Device flash Size : 64KBytes

09:33:

04

: Device family :STM32F303x4-x6-x8/F328xx/F334xx

09:33:

05

: Failed to read memory @08010000!

The programmer seems not to be able to access the microcontroller flash memory. However I can not figure out the reason for this.

If I try to program the microcontroller the following messages are displayed

10:01:45 : [Prova_F334.bin] opened successfully.

10:01:47 : Memory-Loader error

10:01:47 : Error occured during erase operation!

The option bytes are set according to the attached file.

Can anyone help to solve this problem?

Thanks.

#memory-map #stm32f334 #program-memory #flash-corrupt #memory-configuration
This topic has been closed for replies.