Skip to main content
dwarnke
Associate II
July 15, 2014
Solved

IO Function Switching

  • July 15, 2014
  • 1 reply
  • 894 views
Posted on July 15, 2014 at 21:38

I have a project that requires an IO pin to switch between High Z (Tri-State) and High. On a previous 8 bit micro the high z condition was satisfied by setting the port to an input and the high was satisfied by making the port and output and driving it high.

I am using the Hal drivers for non-OS and am strugglinig to find the commands to do this. I tried doing the following with o results:

// Set Charge to Output and Set High

palSetPadMode(PORT_B, CHARGE, PAL_MODE_OUTPUT_PUSHPULL);

palSetPad(PORT_B, CHARGE);

        

// Delay 5us

//osalThreadSleepMicroseconds(CHARGE_WAIT);

osalThreadSleepMicroseconds(50000);

        

// Set Charge to Input and set to high z

palSetPadMode(PORT_B, CHARGE, PAL_MODE_INPUT);

I played with different delay lengths thinking the scope missed it.

Please let me know if you have any ideas.

Doug

#spc56
    This topic has been closed for replies.
    Best answer by Erwan YVIN
    Posted on July 17, 2014 at 17:54

    Hello Doug ,

    Sorry , at the current time, pal_lld_setpadmode is not  implemented (cf pal_lld.h)

    /**

     * @brief   Pad mode setup.

     * @details This function programs a pad with the specified mode.

     * @note    The @ref PAL provides a default software implementation of this

     *          functionality, implement this function if can optimize it by using

     *          special hardware functionalities or special coding.

     * @note    Programming an unknown or unsupported mode is silently ignored.

     *

     * @param[in] port      port identifier

     * @param[in] pad       pad number within the port

     * @param[in] mode      pad mode

     *

     * @notapi

     */

    #define pal_lld_setpadmode(port, pad, mode)

    we need to write the PCR register in this case.

    it is a change request in PAL LLD side.

    Best Regards

                         Erwan

    1 reply

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    July 17, 2014
    Posted on July 17, 2014 at 17:54

    Hello Doug ,

    Sorry , at the current time, pal_lld_setpadmode is not  implemented (cf pal_lld.h)

    /**

     * @brief   Pad mode setup.

     * @details This function programs a pad with the specified mode.

     * @note    The @ref PAL provides a default software implementation of this

     *          functionality, implement this function if can optimize it by using

     *          special hardware functionalities or special coding.

     * @note    Programming an unknown or unsupported mode is silently ignored.

     *

     * @param[in] port      port identifier

     * @param[in] pad       pad number within the port

     * @param[in] mode      pad mode

     *

     * @notapi

     */

    #define pal_lld_setpadmode(port, pad, mode)

    we need to write the PCR register in this case.

    it is a change request in PAL LLD side.

    Best Regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.