Skip to main content
ace0
Associate II
Nov 24, 2016 9:06 PM UTC
Question

STM32F207 DMA PWM

Posted on November 24, 2016 at 22:06

Hi,

I'm using STM32F207 and I would like to trigger DMA transfer on the falling edge of the PWM (duty cycle).

So, I have configured TIM1 in PWM mode and enabled CC1DE and CCDS bits.

uint8_t outBuffer[16] = {0};

int main(void)

{

    RCC_ClocksTypeDef clocks;

    RCC_GetClocksFreq(&clocks);

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE, ENABLE);

    GPIO_InitTypeDef gpioStruct;

    GPIO_StructInit(&gpioStruct);

    gpioStruct.GPIO_Mode = GPIO_Mode_OUT;

    gpioStruct.GPIO_Pin = GPIO_Pin_All;

    gpioStruct.GPIO_OType = GPIO_OType_PP;

    gpioStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

    gpioStruct.GPIO_Speed = GPIO_Speed_100MHz;

    GPIO_Init(GPIOE, &gpioStruct);

    gpioStruct.GPIO_Pin = GPIO_Pin_9;

    gpioStruct.GPIO_Mode = GPIO_Mode_AF;

    gpioStruct.GPIO_OType = GPIO_OType_PP;

    gpioStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;

    gpioStruct.GPIO_Speed = GPIO_Speed_50MHz;

    GPIO_Init(GPIOE, &gpioStruct);

    /* Connect TIM1 pins to AF */

    GPIO_PinAFConfig(GPIOE, GPIO_PinSource9, GPIO_AF_TIM1);

    for (uint32_t i = 0; i < 15; i+=2)

    {

        outBuffer[i] = 0xAAAA;

        outBuffer[i+1] = ~0xAAAA;

    }

    TIM1_Config(100000);

    DMA2_Config();

    while(1)

    {

      if(TIM_GetFlagStatus(TIM1, TIM_FLAG_CC1) == SET)

      {

          GPIO_ToggleBits(GPIOE, GPIO_Pin_14);

          TIM_ClearFlag(TIM1, TIM_FLAG_CC1);

      }

    }

}

void DMA2_Config(void)

{

    DMA_InitTypeDef DMAInitStruct;

    RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 , ENABLE);

    DMA_DeInit(DMA2_Stream1);

    DMAInitStruct.DMA_Channel = DMA_Channel_6;

    DMAInitStruct.DMA_PeripheralBaseAddr = (uint32_t)(GPIOE_BASE) + 0x14;

    DMAInitStruct.DMA_Memory0BaseAddr = (uint32_t)&outBuffer;

    DMAInitStruct.DMA_DIR = DMA_DIR_MemoryToPeripheral;

    DMAInitStruct.DMA_BufferSize = 16;

    DMAInitStruct.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

    DMAInitStruct.DMA_MemoryInc = DMA_MemoryInc_Enable;

    DMAInitStruct.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;

    DMAInitStruct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;

    DMAInitStruct.DMA_Mode = DMA_Mode_Circular;

    DMAInitStruct.DMA_Priority = DMA_Priority_High;

    DMAInitStruct.DMA_FIFOMode = DMA_FIFOMode_Disable;

    DMAInitStruct.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

    DMAInitStruct.DMA_MemoryBurst = DMA_MemoryBurst_Single;

    DMAInitStruct.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

    DMA_Init(DMA2_Stream1, &DMAInitStruct);

    TIM_DMACmd(TIM1, TIM_DMA_CC1, ENABLE);

    DMA_Cmd(DMA2_Stream1, ENABLE);

    TIM_Cmd(TIM1, ENABLE);

}

But what I get is the DMA transfer triggerd on the Update event...

0690X00000605SsQAI.png

Chanel0...PWM output

Chanel2... one of the GPIO bits controlled by the DMA

Chanel3... toggle pin on CC1IF set

Why is DMA transfer triggered on the Update and not on the Compare event? What am I doing wrong?

Thanks!

#stm32f2-dma-pwm
This topic has been closed for replies.

5 replies

waclawek.jan
Super User
Nov 25, 2016 12:08 AM UTC
Posted on November 25, 2016 at 01:08

Post the content of timer registers.

JW

ace0
ace0Author
Associate II
Nov 28, 2016 6:17 PM UTC
Posted on November 28, 2016 at 19:17

Sorry for the delay, I didn't have the board by my side for a few days...

Here is the content of the TIM1 registers right before enabling the timer

0690X00000605ErQAI.png

waclawek.jan
Super User
Nov 28, 2016 7:30 PM UTC
Posted on November 28, 2016 at 20:30

> CCDS  0x01

Don't.

Bit 3 CCDS: Capture/compare DMA selection

0: CCx DMA request sent when CCx event occurs

1: CCx DMA requests sent when update event occurs

JW

waclawek.jan
Super User
Nov 28, 2016 7:33 PM UTC
Posted on November 28, 2016 at 20:33

I see the source of your confusion.

17.3.9  Output compare mode

 

When a match is found between the capture/compare register and the counter, the output

 

compare function:

 

[...]

 

Sends a DMA request if the corresponding enable bit is set (CCxDE bit in the

 

TIMx_DIER register, CCDS bit in the TIMx_CR2 register for the DMA request

 

selection).

 

Very badly formulated, but sadly it's no surprise.

JW

ace0
ace0Author
Associate II
Nov 28, 2016 10:04 PM UTC
Posted on November 28, 2016 at 23:04

excellent observation :)

thanks, it works now...

btw CCDS basically excludes triggering DMA transfer on CC and Update which means that one can't trigger two different streams with one timer? 

For example if I would like to trigger two DMA transfers, one on the falling end and the other on the rising edge of a PWM (CC and Update) is it feasible with one timer? Doesn't look so...