Question
Generate softaware interrupt..
Posted on June 08, 2015 at 10:48
Hi,
I want to generate a software interrupt,.. ie;when I execute one step it should go to ISR and do some activities.. My scenario.. I'm using RTOS for my application. I am reading data from a FIFO and storing it to a buffer via DMA, so while the DMA is ongoing I want so send some packets via WIFI, but the thing is that for context switching it takes max 1ms which is too much, so if I do the conetxt switch with in ISR it'll be switched in 10microsec... this is why I need to generate a software interrupt Please help me.... #interrupts #!stm32f4-disco #software-irq