Skip to main content
hossam
Associate II
November 27, 2014
Question

clear USART TC flag

  • November 27, 2014
  • 5 replies
  • 3244 views
Posted on November 27, 2014 at 21:20

Hi

I am using USART in Interrupt mode in Tx and Rx.

Rx is working fine

But in Tx I keep getting interrupt.

I just need to get the interrupt once when the data is sent.

but I keep getting the interrupt again and again.

When I check the USART->ISR register I found that TC and TXE flags are always set.

I tried to clear them from flags and inerrupt register but they are not responding to clear instructions.USART_ClearFlag() & USART_ClearITPendingBit()

What should I do?

Salam

Hossam Alzomor

#usart-interrupt-tx-tc-txe
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
November 27, 2014
Posted on November 28, 2014 at 00:14

If you have no data to send you have to disable the TXE interrupt.

      /* Clear the TC bit in the SR register by writing 0 to it */

      USART_ClearFlag(USARTx, USART_FLAG_TC);
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
hossam
hossamAuthor
Associate II
November 29, 2014
Posted on November 29, 2014 at 12:18

Thanks

But I think in order to disable the interrupt I should use

  USART_ITConfig(USART1, USART_IT_TC, DISABLE);

and not

  USART_ClearFlag(USARTx, USART_FLAG_TC);

am I right?

When I try to use   USART_ClearFlag(USARTx, USART_FLAG_TC); from within the USART ISR, the interrupt flag is still set and I keep getting into the USART ISR again and again

Regards

Hossam Alzomor

Tesla DeLorean
Guru
November 29, 2014
Posted on November 29, 2014 at 14:58

I have a very narrow window on what your code is doing.

What interrupts have you enabled on the USART? Then make sure you service the ones you've enabled. The ones you haven't enabled will still have IT bits set in the status, but they won't physically generate interrupts. The most probable reason a USART interrupt re-enters is that TXE is set, and you DON'T write a character to USARTx->DR (SendData), as this is the only why to clear the TXE state properly. Like I said, you need to disable the TXE interrupt if you have no data.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
hossam
hossamAuthor
Associate II
November 30, 2014
Posted on November 30, 2014 at 10:38

according to the  STM32F30xx Standard Peripheral Library section 23.2.17.5 USART_ClearFlag page 557 this function can clear TC flag

and section 23.2.17.7 USART_ClearITPendingBit page 558 it can clear pending TC interrupt

and the other option is to write to Tx data register

''TC flag can be also cleared by

software sequence: a read operation to USART_SR register

(USART_GetFlagStatus()) followed by a write operation to

USART_TDR register (USART_SendData()).''

''TC pending bit can be also cleared

by software sequence: a read operation to USART_SR

register (USART_GetITStatus()) followed by a write operation

to USART_TDR register (USART_SendData()).''

Tesla DeLorean
Guru
November 30, 2014
Posted on November 30, 2014 at 15:02

Fantastic, but what interrupts do you have enabled? What does your initialization and IRQ handler code look like? What behaviour are you observing out side of the debugger?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..