Question
STM32F4 Discovery won't go into DFU bootloader mode
Posted on July 18, 2015 at 00:19
Hi All,
I have two discovery boards. When I go into discovery mode (boot0 high, boot1 low) and then run ''dfu-util -l'' ... with one board I see the devices listed, the other board not .. could this be a faulty board?The ''good'' board was a fresh one just out of the packet. The one that doesn't work I have used before and was programmed via ST-LINK using openosd, that worked fine.But this time I want to use DFU and it does not work on that board. Is there a way I could have destroyed the bootloader with ST-LINK?Thanks, #stm32f4-discovery-dfu