Skip to main content
erazmus
Visitor II
August 8, 2014
Question

STM32F429 minimal schematic

  • August 8, 2014
  • 6 replies
  • 1897 views
Posted on August 08, 2014 at 17:21

Hello!

I'd like to design minimal schematic for STM32F429. I'd like to have all pins connected to goldpins. I want to program through ST-LINK and SWD. Please check my schematic. It's in the attachment.

Thanks!

#stm32f429 #basic-circuit
This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
August 8, 2014
Posted on August 08, 2014 at 17:42

I'd definitely recommend getting NRST to the debug connector, and would strongly suggest providing a standard connector (10-pin SWD or 20-pin JTAG)

Also consider a jumper option for BOOT0, and the ability to power VBAT independently.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NEERAJ GUPTA
Associate III
September 4, 2014
Posted on September 04, 2014 at 09:08

Hi Clive,

i have connected MAX3232 with STM32F429ZIT6 as per schematic attached. i have serial port application ''com port toolkit'' configured at 9600 ,8E1 , having 0x7F to this device , the device is replying 0x7F 0xFF 0xFF instead of 0x79 as instructed by you. Further connecting SWCLK & SWDIO pins to STLINK V2 given on your STM32L1-Discovery kit with jumpers removed from CN3. i tried to access the chip on keil after selecting the debug as STLINK. Only STLINK was detected but this device was not. i have checked all Vss & Vdd connections against short circuit. i have set chip Vdd=3.3VDC which converted from Vcc=5VDC , 2A DC power supply. Please! help me.

________________

Attachments :

repeater.PDF : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Wg&d=%2Fa%2F0X0000000bcr%2Fx2oD6xvySn8P1qqDIKwjyIH1sMzarYia81.LBacxsiU&asPdf=false
NEERAJ GUPTA
Associate III
September 4, 2014
Posted on September 04, 2014 at 10:01

Hi clive,

              I have gone through your various posts. I have connected 2.2uF,50V polarized electrolytic capacitors to both VCAP1 & VCAP2 pin. i hv grounded both from -ve marked terminal. I m not getting ~1.2 V on both , the voltage is fluctuating around 0V. Further, 2.2uF ceramic non-polarized caps are not available in India , all i can do is connecting  two pieces of 1uF non-polarized ceramic caps or connect 100nF cap with 2.2uF,50V polarized electrolytic capacitor in parallel to connect with VCAP pins. Please! suggest & help me to decide which combination will work correctly.    

Tesla DeLorean
Guru
September 4, 2014
Posted on September 04, 2014 at 10:54

I'll take a look at the schematic, but you need to be very sure of the part orientation, and where Pin 1 is.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NEERAJ GUPTA
Associate III
September 4, 2014
Posted on September 04, 2014 at 12:09

Hi Clive,

              yes, i m very much sure about part orientation. I m counting PIN no 1 from left notch found on upper left side of  target chip just below ARM logo.  

NEERAJ GUPTA
Associate III
September 4, 2014
Posted on September 04, 2014 at 13:40

Hi Clive,

I have managed to get 2.2uF ceramic non-polarized cap . but still i m not able to ~1.2 V DC across the VCAP pins. Please! go through my latest schematic. i have tested the circuit against all possible other technical glitches. Please! suggest me what to do.

________________

Attachments :

repeater.PDF : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0iA&d=%2Fa%2F0X0000000bcp%2FHAIq8C8cJXHxL9_7WswPqTrEv9vEA3iEz9Sc7sC0H5Y&asPdf=false