Skip to main content
licencje1
Associate III
December 21, 2017
Question

I2C send only adress block in data transfer

  • December 21, 2017
  • 2 replies
  • 1289 views
Posted on December 21, 2017 at 13:32

Hi,

For few days I am trying to send some data over I2C2 interface. I am working with stm32f072-nucleo board.

Unfortunately something goes wrong because stm32 send only address with no data which should be transfered.

My configuration:

static void

MX_I2C2_Init(

void

)

{

 

LL_I2C_InitTypeDef

I2C_InitStruct

;

 

LL_GPIO_InitTypeDef

GPIO_InitStruct

;

 

/**I2C2 GPIO Configuration 

  PB10   ------> I2C2_SCL

  PB11   ------> I2C2_SDA

  */

 

GPIO_InitStruct.

Pin

=

LL_GPIO_PIN_10

;

 

GPIO_InitStruct.

Mode

=

LL_GPIO_MODE_ALTERNATE

;

 

GPIO_InitStruct.

Speed

=

LL_GPIO_SPEED_FREQ_HIGH

;

 

GPIO_InitStruct.

OutputType

=

LL_GPIO_OUTPUT_OPENDRAIN

;

 

GPIO_InitStruct.

Pull

=

LL_GPIO_PULL_UP

;

 

GPIO_InitStruct.

Alternate

=

LL_GPIO_AF_1

;

 

LL_GPIO_Init(

GPIOB

,

&GPIO_InitStruct)

;

 

GPIO_InitStruct.

Pin

=

LL_GPIO_PIN_11

;

 

GPIO_InitStruct.

Mode

=

LL_GPIO_MODE_ALTERNATE

;

 

GPIO_InitStruct.

Speed

=

LL_GPIO_SPEED_FREQ_HIGH

;

 

GPIO_InitStruct.

OutputType

=

LL_GPIO_OUTPUT_OPENDRAIN

;

 

GPIO_InitStruct.

Pull

=

LL_GPIO_PULL_UP

;

 

GPIO_InitStruct.

Alternate

=

LL_GPIO_AF_1

;

 

LL_GPIO_Init(

GPIOB

,

&GPIO_InitStruct)

;

 

/* Peripheral clock enable */

 

LL_APB1_GRP1_EnableClock(

LL_APB1_GRP1_PERIPH_I2C2

)

;

//  LL_RCC_SetI2CClockSource(LL_RCC_I2C1_CLKSOURCE_SYSCLK);

 

LL_RCC_SetI2CClockSource(

LL_RCC_I2C1_CLKSOURCE_SYSCLK

)

;

   

/**I2C Initialization

    */

 

I2C_InitStruct.

PeripheralMode

=

LL_I2C_MODE_I2C

;

 

I2C_InitStruct.

Timing

=

0x2000090E

;

//0x00901850;//0x2000090E;

 

I2C_InitStruct.

AnalogFilter

=

LL_I2C_ANALOGFILTER_DISABLE

;

//LL_I2C_ANALOGFILTER_ENABLE;

 

I2C_InitStruct.

DigitalFilter

=

0

;

 

I2C_InitStruct.

OwnAddress1

=

0

;

 

I2C_InitStruct.

TypeAcknowledge

=

LL_I2C_ACK

;

 

I2C_InitStruct.

OwnAddrSize

=

LL_I2C_OWNADDRESS1_7BIT

;

//  LL_I2C_Disable(I2C2);

 

LL_I2C_Init(

I2C2

,

&I2C_InitStruct)

;

//

 

LL_I2C_EnableAutoEndMode(

I2C2

)

;

 

LL_I2C_SetOwnAddress2(

I2C2

,

0

,

LL_I2C_OWNADDRESS2_NOMASK

)

;

 

LL_I2C_DisableOwnAddress2(

I2C2

)

;

}

int

main(

void

)

{

  LL_Init()

;

 

SystemClock_Config()

;

 

MX_GPIO_Init()

;

 

MX_I2C2_Init()

;

 

i2c_transfer_init(

0xBB

)

;

}

void

i2c_transfer_init(

uint32_t

slave_addr)

{

 

uint8_t

test[

10

] = {

0xAA

}

;

  LL_I2C_HandleTransfer(

I2C2

,

slave_addr

,

LL_I2C_ADDRSLAVE_7BIT

,

2

,

                           

LL_I2C_MODE_AUTOEND

,

LL_I2C_GENERATE_START_WRITE

)

;

//  while(!(LL_I2C_IsActiveFlag_TXE(I2C2))); // waits forever

 

LL_I2C_TransmitData8(

I2C2

,

test[

0

])

;

 

LL_I2C_TransmitData8(

I2C2

,

test[

0

])

;

}

I am attaching oscillograms which shows that only address is being send.

Thanks in advanced for help!

#i2c-problem #nucleo-f072 #stm32f072
This topic has been closed for replies.

2 replies

stm322399
Senior
December 21, 2017
Posted on December 21, 2017 at 14:18

Signal is very ugly, rising edges are too weak. Check pull-up resistors. it is likely that the slave devices does not answer at all because it is unable to recognize its address.

When this will be fixed, double check that the address send for the transfer is really 0xBB. This 0xbb looks like a seven bit address already shifted left by one bit, make sure that the transfer function does not shift once again.

Geoffrey Furman
Associate
January 2, 2018
Posted on January 02, 2018 at 14:41

He is right. The rising edges are not sharp enough. Pullup resistors are either too large or non-existent. Signals don't need to be square but the tops should start to flatten out. Byte being sent is a write to 0xBA. On the 9th clock is the ACK (acknowledge) bit is 1 (NAK'd) meaning that the slave is not present, the signals are not good enough, or the address (0xBA) is incorrect. Some manufacturers specify the 7-bit address right justified (shifted) which is confusing. Sometimes you have to look at the timing diagrams in the datasheet to know for sure which they mean.