Skip to main content
schperplata
Associate III
August 3, 2016
Question

STM32F051K6T6 hardfault with HAL and SPI

  • August 3, 2016
  • 6 replies
  • 2715 views
Posted on August 03, 2016 at 15:18

Hello,

I've got a project build on custom PCB around STM32F051K6T6. There are a couple of other things on this PCB: ULN2003 driver, CD4511B driver , TLV73333 3.3V regulator and the main ''problem'' NRF24L01+ module, connected through SPI1. Board peripherals and init code are generated with CubeMX software. So far everything worked just well: PWM on gpio, timer 6 for some periodic interrupts, CD4511 7 segment driver... When I tried to connect NRF24L01+ through SPI with custom library (modified tm_nrf library) using SPI HAL drivers, strange things happen. uC halts in Hard Fault Handler after a few SPI transmit and/or receive commands. It halts at in stm32fxx_hal_spi.c file in function

HAL_SPI_Transmit()

at specific line ():


HAL_StatusTypeDef HAL_SPI_Transmit(SPI_HandleTypeDef *hspi, uint8_t *pData, uint16_t Size, uint32_t Timeout){

/*

...other code...

*/

/* Transmit data in 8 Bit mode */

else
{

while
(hspi->TxXferCount > 0){

/* Wait until TXE flag is set to send data */

if
((hspi->Instance->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE){


if
(hspi->TxXferCount > 1){

/* write on the data register in packing mode */

hspi->Instance->DR = *((uint16_t*)hspi->pTxBuffPtr);

hspi->pTxBuffPtr += 
sizeof
(uint16_t);

hspi->TxXferCount -= 2;

}

else
{

*((__IO uint8_t*)&hspi->Instance->DR) = (*hspi->pTxBuffPtr++);

hspi->TxXferCount--;

}

}

else
{

/* Timeout management */

if
((Timeout == 0) || ((Timeout != HAL_MAX_DELAY) && ((HAL_GetTick()-tickstart) >= Timeout))){

errorcode = HAL_TIMEOUT;

goto
error;

}

}

}

}

/*

...other code...

*/

}

... and than halts at HarFault_Handler. 0690X00000605FGQAY.png 0690X00000605QwQAI.png 0690X00000605QmQAI.png This is my first HardFault ever, so I don't really know how to handle it. I've google it alot, tried tochange stack size and played with other SPI settings, but with no success. The same NRF24L01 board works with Arduino, so there must be an error somewhere in my code/pcb. Let me know what additional informations are needed. Thanks! #hal #spi #cubemx #hardfault
This topic has been closed for replies.

6 replies

waclawek.jan
Super User
August 3, 2016
Posted on August 03, 2016 at 16:00

> This is my first HardFault ever, so I don't really know how to handle it.

Breath! Breath! ;) Well I usually examine the disassembly in the vicinity of the offending instruction, plus the state of registers at that moment. We lack that at the moment but if it's true that it's related to this line:

hspi->Instance->DR = *((uint16_t*)hspi->pTxBuffPtr);

then chances are that either

hspi->Instance

points to some funny place or, maybe more probably,

hspi->pTxBuffPtr

is not aligned properly (Cortex-M0 can't perform unaligned accesses). It may be worth noting that there are more faults than just the hardfault, indicating the nature of the fault further, but most of the time there is a common vector for all of them, so you lose that information. > works with Arduino, This word is not to be used in a decent society. JW
schperplata
Associate III
August 7, 2016
Posted on August 07, 2016 at 22:44

Hello. Sorry for late reply, I did see your message, but I was very busy with other things. Anyway. in the mean time I noticed, that almost for sure, this code segment in HAL_SPI_Transmit() function is the problem.

1.
hspi->Instance->DR = *((uint16_t*)hspi->pTxBuffPtr);
2.
hspi->pTxBuffPtr += 
sizeof
(uint16_t);
3.
hspi->TxXferCount -= 2;

I will investigate this problem further tomorrow, but for now, if any of you more experienced guys can take a look at 8-bit mode of thisHAL_SPI_Transmit() function, and check if it is really what it should be. Other functions such asHAL_SPI_TransmitReceive() seems like they don't hardfault microcontroller (so

hspi->Instance

should point to something useful). >> works with Arduino, >This word is not to be used in a decent society. I've read this sentence 300 times and laughed each time :D Thanks!
Tesla DeLorean
Guru
August 7, 2016
Posted on August 07, 2016 at 23:15

8-bit should always be fine, the problem with 16-bit and 32-bit is going to be unaligned addresses, you can't read 16-bit values from ODD addresses. You need to manage carefully the buffers handed to the routines.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
schperplata
Associate III
August 9, 2016
Posted on August 09, 2016 at 09:36

OK, unaligned address would make sense. Anyway, I'm using HAL libraries, which means I shouldn't even know any of these things :) In fact, I do like CubeMX software, so I just hope (or not :)) that this is my mistake somewhere else in code, I don't want to return back to STD_Peripheral libs.

I'm trying to create communication with nrf24l01+ with custom library. I init SPI with CubeMX, and than pass

hspi1

handler to this external file (eg. stm32_nrf24lc) like this:

1.
#include ''stm32f0xx_nrf24lh''
2.
extern

SPI_HandleTypeDef hspi1;

... and than use it as I would do it in main.c

1.
void

NRF_SPI_Write(SPI_HandleTypeDef* SPIx, uint8_t* data_out, uint32_t count) {
2.

HAL_SPI_Transmit(SPIx, data_out, count, SPI_TIMEOUT);
3.
}

I call this function as:

1.
NRF_SPI_Write(&hspi1, data, count);

So, if I change HAL_SPI_Transmit() function to something I would say is logical to avoid unaligned acces (delete ''16-bit mode'' out and use only 8-bit way to transfer data), this is:

...

/* Check if the SPI is already enabled */

if

((hspi->Instance->CR1 & SPI_CR1_SPE) != SPI_CR1_SPE){

/* Enable SPI peripheral */

__HAL_SPI_ENABLE(hspi);

}

// EDITED 9.8.2016 ***********************************************

while

(hspi->TxXferCount > 0){

/* Wait until TXE flag is set to send data */

if

((hspi->Instance->SR & SPI_FLAG_TXE) == SPI_FLAG_TXE){

*((__IO uint8_t*)&hspi->Instance->DR) = (*hspi->pTxBuffPtr++);

hspi->TxXferCount--;

}

else

{

/* Timeout management */

if

((Timeout == 0) || ((Timeout != HAL_MAX_DELAY) && ((HAL_GetTick()-tickstart) >= Timeout))) {

errorcode = HAL_TIMEOUT;

goto

error;

}

}

}


/* Enable CRC Transmission */

if

(hspi->Init.CRCCalculation == SPI_CRCCALCULATION_ENABLE){


...

(It is just deleted ''packaging transfer mode''). Well, this is also not working, but at least uC don't lock in HardFault. Any ideas what I am doing wrong? Is it possible this is some kind of HAL_SPI driver bug? I didn't have any real problems with CubeMX generated code so far. Also, time for my project is running really low, and I can't do anything further without nrf24l01+ communication. Thanks!
waclawek.jan
Super User
August 9, 2016
Posted on August 09, 2016 at 10:06

> Well, this is also not working

Specify.

JW
schperplata
Associate III
August 9, 2016
Posted on August 09, 2016 at 11:28

I've just figured out that two boards, configured as full duplex master - slave can normally communicate through SPI with default CubeMX software. This means an error must be somewhere in nrf24l01+ library or passed arguments that cause unaligment.

> Well, this is also not working

 

It doesn't cause HardFault, and no SPI status error is generated, but other code concerning nrf24l01 is not working - it says 1 byte is always available even with no nrf module attached. Anyway, I will focus now on nrf library and arguments to HAL_SPI functions as mentioned above.