Skip to main content
Dimitris Paraskevopoulos
Associate III
March 4, 2018
Question

Hungarian notation on USB code

  • March 4, 2018
  • 4 replies
  • 1078 views
Posted on March 04, 2018 at 15:35

If I am not mistaken some variables on the USB code use hungarian notation e.g. bRequest, wValue, wIndex etc.

However there is one prefix that I don't know what it means bmRequest.

Is it something like multiple bits because it is like a bitfield?

Is there a link that explains the conventions used? Are there any other non standard ones that I may not have spotted yet.

Cheers,

Sat

#hungarian #notation #usb #stm32-stm32cube
This topic has been closed for replies.

4 replies

Bogdan Golab
Lead
March 4, 2018
Dimitris Paraskevopoulos
Associate III
March 4, 2018
Posted on March 04, 2018 at 15:53

My question is coming from this document. I am asking about the prefix not what the variable does.

Bogdan Golab
Lead
March 4, 2018
Posted on March 04, 2018 at 16:28

Sorry I miss-interpreted the sentence: 'I don't know what it means bmRequest.'

waclawek.jan
Super User
March 4, 2018
Posted on March 04, 2018 at 17:15

The notation matches that of USB specification (Microsoft played part in developing it, and Simonyi developed that notation while at Microsoft, the years roughly match), see the dreaded chapter 9. It does not strictly denote type - while b is for byte and w is for [16-bit] word, bm is there for bitmap (an item where individual bits or groups of few bits have ditinct meanings, in the basic document it's usually byte but in class documents there are multiple-byte bitmaps, too), i for index (the only usage I've seen is index to the strings pool, a byte), bcd for binary-coded-decimal (usually version number and it's usually two bytes).

JW