Skip to main content
GS1
Senior III
July 5, 2018
Question

Need Flash Algorithm for S25FL256S Flash Device or similar for STM32H743i

  • July 5, 2018
  • 1 reply
  • 730 views
Posted on July 05, 2018 at 19:36

Hello all,

I am urgently looking for a Flash Programming Algorithm for the S25FL256S or S25FL512S Quad SPI Flash Device. This device will be used on a board with an STM32H743i processor. I use Keil as Development Environment and need a Flash Programming Algorithm for the ULINK / ST Link Programming of the system.

Alternatively we could use the MT25QL512ABA Device from Micron.

It seems that there is currently no Flash Algorithm available for Keil.

I tried to find a similar flash programming algorithm which I could use as a base to develop on, but didn't find something up to now.

Has anybody set up a flash programming algorithm for a similar or same device which I can hook to?

Any help very much appreciated!

Gaby

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 5, 2018
    Posted on July 05, 2018 at 23:22

    I'd be open to reasonable offers for my time.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..