Skip to main content
sgetz
Visitor II
December 5, 2014
Question

LIS3DSH Power Down Current

  • December 5, 2014
  • 1 reply
  • 663 views
Posted on December 05, 2014 at 21:12

I only seem to be able to power the LIS3DSH down to about 70uA by writing a 0x00 to CTRL_REG4 (0x20).

CS is High.

SEL is Low.

I am using I2C.

Running at 2.5V

What do I need to do to get to the spec power down current?

#lis3dsh-power-down-current
This topic has been closed for replies.

1 reply

mharvey
Visitor II
March 19, 2015
Posted on March 19, 2015 at 19:38

I am betting that the LIS3DSH is like the LIS3DH and that the I2C address select pin has an internal Pull Up resistor.  Since you are grounding that pin you have an extra current flowing through that pin.  We confirmed this on the LIS3DH.