Skip to main content
jjonethal
Associate II
November 2, 2015
Question

STM32F3Discovery SB13 and SB15 for VCP via USB ?

  • November 2, 2015
  • 3 replies
  • 780 views
Posted on November 02, 2015 at 21:15

Is there a way to use uart on stm32f103c8t6 for VCP over debugging chip or is there

a flash limitation for debugger firmware ? For Nucleo411 there is VCP support via STM32F103CBT6 which has twice as much flash as the debug chip on the f3discovery.

Any Ideas ?

Kind Regards Jean
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    November 2, 2015
    Posted on November 02, 2015 at 22:09

    Most DISCO boards don't support the VCP functionality.

    The new STM32F469I-DISCO also has an STM32F103CBT6 and supports both the mbed and VCP functionality.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jjonethal
    jjonethalAuthor
    Associate II
    November 3, 2015
    Posted on November 03, 2015 at 09:18

    Dear clive1,

    Thank you for the fast response.

    is it possible to flash the Stm32f3discovery debugger with the STM32F469I-DISCO debugger image ?

    jjonethal
    jjonethalAuthor
    Associate II
    November 5, 2015
    Posted on November 05, 2015 at 15:16

    I've tried to burn f2_4.bin from 411nucleo into the STM32F3Discovery board. After burning f2_4.bin Windows started to install the VCP driver but afterwards debugging was not possible. So i burned f2_1.bin and my debugger was alive again. I guess it's faster to use another open source alternative.