Question
Using Eclipse IDE with Nucleo-F103RB (STM32F103) F1 series
Posted on September 08, 2014 at 15:36
I've previously being using an Cortex-M3 STM32F105RC to evaluate a project, but I have since purchased a Cotex-M4 Nucleo-F103RB development board and aim to port the project over to the new MCU.
I previously had the project running in eclipse using Sourcery CodeBench Lite for ARM EABI (arm-none-eabi-gcc) and would like to know if I can use this toolchain again to setup a project for the new Nucleo-F103RB microcontroller. If this is possible is there a guide to setting this up/any differences to my previous setup e.g. specifying the FPU type, instruction set? Also, previously I needed the compiler symbols: STM32F10X_CL and USE_STDPERIPH_DRIVER. I will be needing the STM32_Nucleo_FW_V1.2.1 libraries, so would the new project require the symbols: STM32F10X_MD and USE_STDPERIPH_DRIVER, anything else?Thanks #stm32f103rb #nucleo #eclipse