Skip to main content
massimiliano
Visitor II
September 12, 2014
Question

L6472 homing best pratice

  • September 12, 2014
  • 3 replies
  • 774 views
Posted on September 12, 2014 at 11:22

Hi,

I'm wondering what is the best approach to proceed with homing, let's say we have two limit switches CW and CCW, when system starts and none of them are pressed it's easy to proceed with homing, i.e moving to CW direction, find lower limits, reset ABS register, move towards CCW and find upper limits,

but what if when system starts, for any reason,  one of two limit switches are already pressed?

there is only one SW pin on L6472,  CW and CCW limit switches are usually  to be connected in parallel, what is the right direction for release the switch?

Actually to solve this dilemma i've used this workaround, add redundant MCU GPIO pins to limit switches, to check any limits before starting homing procedure.

I'm wondering if there a more smarter way (i.e. check motor current or whatever) to resolve this issues.

Best Regards

Massimiliano
This topic has been closed for replies.

3 replies

Enrico Poli
ST Employee
September 23, 2014
Posted on September 23, 2014 at 08:36

Hi Massimiliano,

I think you can avoid the extra GPIO. You can try with this procedure:

1. check the SW status through the STATUS register of the L6472

2. if the SW input is forced low try performing a small movement in CW (or CCW) direction

3. if the SW is released that means that the limit sitch forcing the signal is the CW (or CCW) one, otherwise it is the opposite.

4. proceed with the normal homing strategy

Take care that the L6472, by default, cause an hardstop when the SW input is forced low, so if the input is low at power-up the power stage is enabled and you need to set it in high impedance before setting the configuration parameters.

Regards

Enrico

Lorenzo1
Associate
April 2, 2015
Posted on April 02, 2015 at 21:15

Hi Enrico,

about the last line in your last message...

There is a way to avoid the power stage to switch ON even if SW is low at power-up?

This because I want to eliminate the small time between the stage enabling at start-up and my disable command.

Thanks, Lorenzo

Enrico Poli
ST Employee
April 8, 2015
Posted on April 08, 2015 at 11:56

Hi Lorenzo,

Unfortunately it is an automatic procedure. There is no way to disable it.

You can use one GPIO of your MCU to temporary bypass the limit switch as described in the attached schematic.

Keeping the GPIO output high until the automatic HardStop is disabled should avoid the power stage turn-on. As soon as the configuraton is changed, the GPIO must be disabled (high impedance).

Regadrs

Ernico

________________

Attachments :

example.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzGa&d=%2Fa%2F0X0000000bJJ%2FNBk9KPgJxlxoDcsz83DSl5me7sovajQYCxDU3Pyby_g&asPdf=false