Skip to main content
intcd31
Associate II
February 13, 2015
Question

ADC_TripleMode_RegSimult data corruption

  • February 13, 2015
  • 2 replies
  • 660 views
Posted on February 13, 2015 at 16:45

I am using stm32f427 chip with external SDRAM. I tried to implement ADC triple mode but I found the raw data transferred to external memory by DMA is duplicated or corrupted.

#define SDRAM_BANK1_1MB_ADDR      (0xC0100000)

void SetupADC_Receive(void)

{

    ADC_InitTypeDef ADC_InitStructure;

    DMA_Cmd(DMA2_Stream0, DISABLE);

    // Disable the sampling ADC's 

    ADC_Cmd(ADC1, DISABLE);

    ADC_Cmd(ADC2, DISABLE);

    ADC_Cmd(ADC3, DISABLE);

    // Disable the ADC's DMA interface

    ADC_DMACmd(ADC1, DISABLE);

    ADC_DMACmd(ADC2, DISABLE);

    ADC_DMACmd(ADC3, DISABLE);

    // Configure the DMA for the sampling (also enables the DMA).

    SetupDMA();

    

    SetupADC_common();

    ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

    ADC_InitStructure.ADC_ScanConvMode = ENABLE;

    ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

    ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_Rising;

    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T5_CC1;

    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

    ADC_InitStructure.ADC_NbrOfConversion = 3;

    {

        ADC_Init(ADC1, &ADC_InitStructure);

        ADC_DiscModeChannelCountConfig(ADC1, 3);

        ADC_DiscModeCmd(ADC1, ENABLE);

        // ADC Regular Channel Configuration 

        ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1, ADC_SampleTime_3Cycles);

        ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 2, ADC_SampleTime_3Cycles);

        ADC_RegularChannelConfig(ADC1, ADC_Channel_15, 3, ADC_SampleTime_3Cycles);

    }

    {

        ADC_Init(ADC2, &ADC_InitStructure);

        // ADC Regular Channel Configuration 

        ADC_RegularChannelConfig(ADC2, ADC_Channel_1, 1, ADC_SampleTime_3Cycles);

        ADC_RegularChannelConfig(ADC2, ADC_Channel_14, 2, ADC_SampleTime_3Cycles);

        // NOT USED -- for interleaving alignment

        ADC_RegularChannelConfig(ADC2, ADC_Channel_2, 3, ADC_SampleTime_3Cycles);

    }

    {

        ADC_Init(ADC3, &ADC_InitStructure);

        // ADC Regular Channel Configuration 

        ADC_RegularChannelConfig(ADC3, ADC_Channel_4, 1, ADC_SampleTime_3Cycles);

        ADC_RegularChannelConfig(ADC3, ADC_Channel_5, 2, ADC_SampleTime_3Cycles);

        // NOT USED -- for interleaving alignment

        ADC_RegularChannelConfig(ADC3, ADC_Channel_8, 3, ADC_SampleTime_3Cycles);

    }

    ADC_DMACmd(ADC1, ENABLE);

    // Enable the sampling ADC's

    ADC_Cmd(ADC2, ENABLE);

    ADC_Cmd(ADC3, ENABLE);

    ADC_Cmd(ADC1, ENABLE);

}

void SetupDMA(void)

{

    DMA_InitTypeDef DMA_InitStructure;

    DMA_DeInit(DMA2_Stream0);

    ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);

    DMA_Cmd(DMA2_Stream0, DISABLE);

    DMA_InitStructure.DMA_Channel = DMA_Channel_0;

    DMA_InitStructure.DMA_PeripheralBaseAddr = ((uint32_t)(&ADC->CDR));

    DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

    DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)SDRAM_BANK1_1MB_ADDR;

    DMA_InitStructure.DMA_BufferSize = 0x1800 * 3;

    DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

    DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

    DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

    DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

    DMA_InitStructure.DMA_Mode = DMA_Mode_Normal;//DMA_Mode_Circular;//

    DMA_InitStructure.DMA_Priority = DMA_Priority_VeryHigh;

    DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;

    DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

    DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

    DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

    DMA_Init(DMA2_Stream0, &DMA_InitStructure);

    // Enable DMA stream.

    DMA_Cmd(DMA2_Stream0, ENABLE);

}

void SetupADC_common(void)

{

    // Initialize the ADC common registers.

    ADC_CommonInitTypeDef ADC_CommonInitStructure;

    ADC_CommonInitStructure.ADC_Mode = ADC_TripleMode_RegSimult;

    ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

    ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_1;

    ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

    ADC_CommonInit(&ADC_CommonInitStructure);

}

Here is the dump. From C01000000, we can see the duplicated data.

0690X00000605EgQAI.png

What confused me is that I did ADC_Mode_Independent ADC_DMAAccessMode_Disabled only to transfer ADC1 data and the data is totally correct. From my point of view, it should be some part related to ADC common where I set it wrong. Can somebody help me find out this? 
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    February 13, 2015
    Posted on February 13, 2015 at 17:25

    Try one of the example of this that I've posted and confirm if that does, or does not, function correctly with a SDRAM destination. I don't really have the time/patience to keep fixing everyone's broken code. Start with something that works, then push that till it breaks.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    intcd31
    intcd31Author
    Associate II
    February 16, 2015
    Posted on February 16, 2015 at 18:13

    ok The problem is fixed. It needs to put the code below.

    ADC_MultiModeDMARequestAfterLastTransferCmd(ENABLE);

    Thanks anyway.