Skip to main content
davide
Associate III
June 8, 2017
Question

HAL UART DMA circular buffer TX/RX

  • June 8, 2017
  • 4 replies
  • 1639 views
Posted on June 08, 2017 at 10:58

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    4 replies

    davide
    davideAuthor
    Associate III
    June 11, 2017
    Posted on June 11, 2017 at 10:53

    Hi there,

    further investigation pointed towards a strange behaviour:

    the aforementioned code is working great if it's compiled with -O0, 1, 2, 3, g, s but HAL_UART_RECEIVE_DMA fails to set the uart peripheral in UART_STATE_BUSY_RX when the gcc optimisation is settled to -Of, hence the issue i have enlightened in the previous post.

    It that a known behaivour of Hal_Uart, there's a solution the this issue?

    ty! 

    Davide

    waclawek.jan
    Super User
    June 11, 2017
    Posted on June 11, 2017 at 11:24

    Issues related to variables modified in interrupts and having different behaviour upon aggressive optimization tend to be related to insufficient use of the volatile qualifier.

    I don't Cube.

    JW

    davide
    davideAuthor
    Associate III
    June 11, 2017
    Posted on June 11, 2017 at 20:11

    Thanks waclawek.jan,

    unfortunately also i have always used SPL, but this project requires HAL: a good opportunity to know better these drivers but also an effort to adapt to a very different point of view. 

    It's a pity that this simple thing isn't working out of the box with any optimisation, after all i've written the code in a very naive way: only hal irq handlers are used inside the isr services, as also done by mx cube.

    Davide

    ps: any further info is well accepted, also if there is a way to point out this issue to the hal drivers team i'll be happy to contribute!

    Jari Nippula
    Visitor II
    October 19, 2017
    Posted on October 19, 2017 at 08:18

    Your Rx DMA seems to use Channel3 without interrupt enable call and int handler.

    Jari