Skip to main content
emil
Associate II
November 24, 2017
Question

Bug in CubeMX - incorrect audio frequency

Posted on November 24, 2017 at 03:20

In CubeMX version 4.23.0 when using  a I2S interface with a STM32F405 processor:

- under parameter settings tab the 'Real Audio Frequency' is not updated correctly when you change the 'R' divider from the I2S PLL; the 'N' multiplier however does update the frequency.

    This topic has been closed for replies.

    1 reply

    emil
    emilAuthor
    Associate II
    December 15, 2017
    Posted on December 15, 2017 at 16:17

    What actually happens is that the I2S PLL multiplier and divider are not changed automatically to minimize your sample rate error.

    If this is a bug or not might be debatable. In the end I wrote a little C program to get the best N,R combination for a given sample rate.

    What is a bug though is the error calculation: With 1MHz input frequency into the I2S PLL the best combination for N,R is

    Frequency 44099.508 error -0.0011% N 429 R 4 I2SDiv 38

    If you put in the I2S configuration 'Custom Freq' and 44100Hz the frequency is calculated correctly as 44.099KHz but

    'Error between Selected and Real' is displayed as 0.22% which is clearly an error.