Skip to main content
oli
Associate III
August 21, 2015
Question

STM32F4 Input Capture TIM2 Channel 4

  • August 21, 2015
  • 1 reply
  • 636 views
Posted on August 21, 2015 at 14:02

Hello

I'm faced to the Problem that I do have to use TIM2 channel 4 for Input capture.

I know that channel 4 can not be used like 1 to 3.

But I thaught I can use the channel 4 to get edges and take CCR4 as counter to take its value each time I detect an positive edge.

I get an IRQ each time a positive edge occurres but CCR4 doesn't count up.

To compare the behaviour I'm using TIM3 channel 1 where it works well with the same configuration (of course TIMx is different) as simple input capture.

Does anyone know where the difference can be?

Thanks

#stm32
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    August 21, 2015
    Posted on August 21, 2015 at 16:49

    It should latch the current counter value, but it doesn't intrinsically ''count''. Determine why the counter isn't advancing.

    I can't deduce what you're doing wrong with the details you've provided.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..