Skip to main content
siddj
Associate III
May 17, 2009
Question

Timer Config.

  • May 17, 2009
  • 2 replies
  • 688 views
Posted on May 17, 2009 at 16:03

Timer Config.

    This topic has been closed for replies.

    2 replies

    amin2
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:07

    hi ,

    Take a look on the STM8S Firmware TIM1 example ''TIM1_Input_Capture'',

    it calculate the frequency of an external signal.

    STM8S and STM32 Timers are compatible and the Firmwares are 99% similar.

    link is :

    http://www.st.com/products/support/micro/files/stm8sfwlib.zip

    Amin

    [ This message was edited by: amin.agina on 17-05-2009 19:34 ]

    siddj
    siddjAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:07

    Hey everyone,

    I am using the STM32F103 VE chip in my project. I need to be able to record the timing between to events to measure the speed of a device. When I get an external interrupt on one of my GPIO's I know that a wheel has moved x inches. So, every time I get this interrupt I would want to start a counter and then stop , record the difference and start the timer again.

    More specifically one of my GPIO pins will be high and when i get an interrupt it will be pulled low, signaling the fact that the wheel has moved x inches. Then I clear the interrupt and the same thing continues. I have TIM8 on that pin. I was wondering what configuration would be most suitable to get the time difference between the two events.

    Thanks for your help!

    -Regards.