Skip to main content
scholar
Associate II
February 13, 2015
Question

stm32f4 + ov7670 + dmlcd-35rt double upscaled image

  • February 13, 2015
  • 0 replies
  • 617 views
Posted on February 13, 2015 at 03:16

i am working on a project with stm32f4 , ov7670  and dm-lcd35rt image output from my camera is doubled and also its colour is greenish  following is my register setting

// Clock Settings // xclk 24M pclk 12M

    {0x11, 0x00}, // 

    {0x6b, 0x8a}, // 

// check different 

{0x3a, 0x08},

{0x3d, 0xc2},

  {0x12, 0x15}, // RGB processed  set + QVGA set

  {0x40, 0xd0}, // output range till 0xFF RGB-565 select

{0x3e, 0x11},

in snapshot mode it works fine but in continuous mode frame overlaps i cant work out why frames are overlaping in such way

on each vsync interrupt i set my lcd cursor to 0,0 apparantly it is not working this way following is my intterupt function

void DCMI_IRQHandler(void)

{     

if (DCMI_GetITStatus(DCMI_IT_VSYNC) != RESET) 

{   

LCD_SetCursor(0,0);

LCD_WriteRAM_Prepare();

DCMI_ClearITPendingBit(DCMI_IT_VSYNC);  

}

if (DCMI_GetITStatus(DCMI_IT_LINE) != RESET) 

{

DCMI_ClearITPendingBit(DCMI_IT_LINE);  

}

if (DCMI_GetITStatus(DCMI_IT_FRAME) != RESET) 

{

DCMI_ClearITPendingBit(DCMI_IT_FRAME);

}

if (DCMI_GetITStatus(DCMI_IT_ERR) != RESET) 

{

DCMI_ClearITPendingBit(DCMI_IT_ERR);

}

}

image from my lcd output is attached 

can any one give me some directions about it?
    This topic has been closed for replies.