Associate
February 9, 2015
Question
STM32f2xx SWD programmer problem
- February 9, 2015
- 3 replies
- 1085 views
Posted on February 09, 2015 at 16:34
Hi at all,
I would try to program a custom made board with STM32f205RCT7 micro onboard via SWD .I got an SWD connector with vdd,gnd,swdio,swclk,nrst.No pull up or pull down on swdio pin , 10k ohm pull up on nrst and 1nF to GND.10k ohm pull down on BOOT 0 .I am use STM32 ST-LINK utility ( Connection protocol SWD).This is the message I get :15:11:46 : ST-LINK Firmware version : V2J22S415:11:46 : Connected via SWD.15:11:46 : Connetion mode : Connect Under Reset.15:11:46 : Device ID:0x411 15:11:46 : Device flash Size : 256KBytes15:11:46 : Device family :STM32F2xx15:11:46 : Can not connect to device!I tried to remove nrst 1nF capacitor but it did not help.I tried on 2 different boards, is it the same problem.The Vcc is OK. Vcap_1 and Vcap_2 1.2 V . I am check swdio,swclk,nrst with oscilloscope and it looks good.I have another board (very same to the first , base on STM32f205RCT6 and SWD connection too) and its work perfect in the same setup.