Skip to main content
270284440
Associate II
June 25, 2015
Question

[solved]Pictus input pin selection

  • June 25, 2015
  • 2 replies
  • 877 views
Posted on June 25, 2015 at 11:45

Hello,

Please see attached pictures cut from pictus RM0022 page 86.

There are two input fucntion selectable of A[8] pin, SIN, and EIRQ[8].

I read and understand that to select input function , PCR.IBE = 1 must be set,

but how to set SIN and EIRQ ? by configure in PSMI register or

function of SIN and EIRQ are connected internally in the MCU chip?

Thanks so much!

#pcr-pictus
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    July 2, 2015
    Posted on July 02, 2015 at 16:11

    Hello Chu ,

    No need to use PSMI.

    IBE to 1 on A[8] is enough to enable SIN_1 and EIRQ_8

    SIN_1 and EIRQ_8 are connected in an intrinsic function.

    Best regards

                         Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    270284440
    270284440Author
    Associate II
    July 3, 2015
    Posted on July 03, 2015 at 03:42

    Hi ,Erwan.

    Thank you so much!