Skip to main content
mw876
Visitor II
February 13, 2015
Question

I2C Issues Using STM32F429I Discovery Board.

  • February 13, 2015
  • 1 reply
  • 627 views
Posted on February 13, 2015 at 13:23

I am attempting to configure the pins on the STM32F429I Discovery Board so that i can connect some I2C sensors and produce some data readings for a project i am working on.

I am using the template file given by ST for this Discoveruy Board using Keil uvision 5. Using an oscilloscope it appears that during the initialisation of the GPIO pins the SCL pin pb6 attempts to go high and then something pulls it low again meaining that the I2C assumes that the line is busy and wont communicate with the board. I think i am performing the setup corectly. Any Help would be greatly appreciated. Here is the code i have written so far.

#include ''i2c.h'' 
#include ''stm32f4xx_conf.h'' 
#include ''stm32f4xx_i2c.h'' 
#include ''stm32f4xx_gpio.h'' 

void
i2c_init(
void
){ 
GPIO_InitTypeDef GPIO_InitStruct; 
// this is for the GPIO pins used as I2C1SDA and I2C1SCL 
I2C_InitTypeDef I2C_InitStruct; 
// this is for the I2C1 initilization 
/* Enable Clocks */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE); 
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); 
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; 
// Pins 6(I2C1_SCL) and 7(I2C1_SDA) 
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; 
// the pins are configured as alternate function so the USART peripheral has access to them 
GPIO_InitStruct.GPIO_Speed = GPIO_Speed_100MHz;
// this defines the IO speed and has nothing to do with the baudrate! 
GPIO_InitStruct.GPIO_OType = GPIO_OType_OD;
// this defines the output type as open drain 
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_UP;
// this activates the pullup resistors on the IO pins 
GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1); 
// 
GPIO_PinAFConfig(GPIOB, GPIO_PinSource7, GPIO_AF_I2C1); 
GPIO_Init(GPIOB, &GPIO_InitStruct);
// now all the values are passed to the GPIO_Init() 
/* Set the I2C structure parameters */
I2C_InitStruct.I2C_Mode = I2C_Mode_I2C; 
I2C_InitStruct.I2C_DutyCycle = I2C_DutyCycle_2; 
I2C_InitStruct.I2C_OwnAddress1 = 0x00; 
I2C_InitStruct.I2C_Ack = I2C_Ack_Enable; 
I2C_InitStruct.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; 
I2C_InitStruct.I2C_ClockSpeed = 100000; 
I2C_Cmd(I2C1, DISABLE); 
I2C_Init(I2C1,&I2C_InitStruct); 
I2C_Cmd(I2C1, ENABLE); 
} 
uint8_t SHT21_ADR = 0x40; 
uint8_t TCS3472_ADR = 0x29; 
double
Read_Sensor(
int
parameter) 
{ 
uint32_t timeout = I2C_IT_TIMEOUT; 
uint16_t data = 0; 
uint8_t command = 0; 
uint8_t address = 0; 
double
value = 0xFF; 
/*Possible Sensor Calculations*/
switch
(parameter){ 
case
TEMPERATURE: 
command = 227; 
address = SHT21_ADR; 
break
; 
case
HUMIDITY: 
command = 229; 
address = SHT21_ADR; 
break
; 
case
RED: 
address = TCS3472_ADR; 
break
; 
case
GREEN: 
address = TCS3472_ADR; 
break
; 
case
BLUE: 
address = TCS3472_ADR; 
break
; 
default
: 
return
0xFF; 
} 
/* Generate the Start Condition */
while
(I2C_GetFlagStatus(I2C1,I2C_FLAG_BUSY)); 
I2C_GenerateSTART(I2C1, ENABLE); 
/* Test on I2C1 EV5 and clear it */
while
(!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); 
// { 
// /* If the timeout delay is exceeded, exit with error code */ 
// if ((timeout--) == 0){ 
// return 0xFF; 
// } 
// } 
I2C_Send7bitAddress(I2C2, address, I2C_Direction_Transmitter); 
/* Test on I2C1 EV6 and clear it */
timeout = I2C_IT_TIMEOUT; 
/* Initialize timeout value */
while
(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)) 
{ 
/* If the timeout delay is exeeded, exit with error code */
if
((timeout--) == 0){ 
return
0xFF; 
} 
} 
I2C_SendData(I2C2,command); 
/* Test on I2C1 EV8 and clear it */
timeout = I2C_IT_TIMEOUT; 
/* Initialize timeout value */
while
(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_TRANSMITTED)){ 
/* If the timeout delay is exeeded, exit with error code */
if
((timeout--) == 0) 
return
0xFF; 
} 
/* Generate the Start Condition */
I2C_GenerateSTART(I2C2, ENABLE); 
/* Test on I2C1 EV6 and clear it */
timeout = I2C_IT_TIMEOUT; 
/* Initialize timeout value */
while
(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_MODE_SELECT)) 
{ 
/* If the timeout delay is exeeded, exit with error code */
if
((timeout--) == 0) 
return
0xFF; 
} 
I2C_Send7bitAddress(I2C2, SHT21_ADR ,I2C_Direction_Receiver); 
/* Test on I2C1 EV6 and clear it */
timeout = I2C_IT_TIMEOUT; 
/* Initialize timeout value */
while
(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)) 
{ 
/* If the timeout delay is exeeded, exit with error code */
if
((timeout--) == 0) 
return
0xFF; 
} 
I2C_AcknowledgeConfig(I2C2, ENABLE); 
/* Test on I2C1 EV6 and clear it */
timeout = I2C_IT_TIMEOUT; 
/* Initialize timeout value */
while
(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)) 
{ 
/* If the timeout delay is exeeded, exit with error code */
if
((timeout--) == 0) 
return
0xFF; 
} 
data = I2C_ReceiveData(I2C2); 
data = data<<8; 
/* Prepare an NACK for the next data received */
I2C_AcknowledgeConfig(I2C2, DISABLE); 
timeout = I2C_IT_TIMEOUT; 
/* Initialize timeout value */
while
(!I2C_CheckEvent(I2C2, I2C_EVENT_MASTER_BYTE_RECEIVED)) 
{ 
/* If the timeout delay is exeeded, exit with error code */
if
((timeout--) == 0) 
return
0xFF; 
} 
I2C_GenerateSTOP(I2C2, ENABLE); 
data |= I2C_ReceiveData(I2C2); 
/*Bit mask the LSB bits to Zero based on the type of measurement made */
if
(parameter == TEMPERATURE){ 
data = data & (0xFFFC); 
//Last 2 Bits are set to Zero 
value = convertTemperature(data); 
} 
else
if
(parameter == HUMIDITY){ 
data = data & (0xFFF0); 
value = convertHumidity(data); 
} 
else
if
(parameter == RED || parameter == GREEN || parameter == BLUE){ 
uint16_t buffer = data &0x00FF; 
buffer = buffer<<8; 
data = (data>>8) &0x00FF; 
data = buffer | data; 
value = data; 
} 
return
value; 
} 
double
convertTemperature(uint16_t data){ 
double
value; 
value = data * 72 / 65536 - 65; 
return
value; 
} 
double
convertHumidity(uint16_t data){ 
double
value; 
value = data * 125 / 65536 - 6; 
return
value; 
} 

    This topic has been closed for replies.

    1 reply

    Amel NASRI
    ST Technical Moderator
    March 4, 2015
    Posted on March 04, 2015 at 09:09

    Hi,

    Please move ''

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1, ENABLE);'' call after ''

    GPIO_Init(GPIOB, &GPIO_InitStruct);''.

    Let me know if this fixes your issue.

    -Mayla-

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.