2016-01-25 4:51 PM
Does anyone know if its possible to output TIM3 on an I/O pin to view or trigger another external device? I noticed the absence of the BDTR register for TIM3 and the MOE bit in the register map bit fields. If there another method which a TIM3 register should be used to output a signal on an I/O pin?
2016-01-25 5:15 PM
Yeah, pretty sure you just put it in Output Compare, or PWM1/PMW2 mode. It is not a ''special'' timer like TIM1/TIM8, so no PWM Output Enable required, or Break features
Check the TIM3_CHx pins for your specific device configurationhttp://www.st.com/web/en/resource/technical/document/datasheet/DM00088500.pdf