Visitor II
March 4, 2015
Question
STM32CubeMX Clock Configuration Problem
- March 4, 2015
- 1 reply
- 893 views
Posted on March 04, 2015 at 23:44
I'm trying to use Cube for an STM32F042 project and I'd like the APB1 peripheral clock to be 1 MHz but Cube is saying that the minimum APB1 peripheral clock is 10 MHz. Is this true or is this a problem with Cube? If it does need to be 10MHz or higher where does it say this in the documentation, I couldn't find it.
I've included a screen shot of the parameters and the red box. Thanks, Jeff