Skip to main content
didattica2
Associate
March 11, 2015
Question

FreeRTOS + LwIP on STM32F407VG Discovery

  • March 11, 2015
  • 3 replies
  • 897 views
Posted on March 11, 2015 at 20:34

Hi,

I'm new to LwIP and I'm trying to run it on STM32F4 Discovery with FreeRTOS. I'm using STM32CubeMX for generating default code and System Workbench (AC6) as IDE. I use DP83848 PHY in RMII mode. 

All the software works great (e.g pinging the board, or run the web server demo) if no FreeRTOS is used. But when I add FreeRTOS the board does not acquire a valid IP (either via DHCP or with static IP) so it is not possible to ping the board. This even if I do not add any code to the STM32Cube generated code 

Thanks in advance if you can help me

    This topic has been closed for replies.

    3 replies

    didattica2
    Associate
    March 15, 2015
    Posted on March 15, 2015 at 19:35

    Problem solved.

    Simply add this line to lwipopts.h (1000 or whatewer value but > 0):

     #define TCPIP_THREAD_STACKSIZE          1000

    If not specified, the default value is 0 (see opt.h) but in that case no lwIp threads is created: this not seems normal for me if I want to use an RTOS.

    Comments are welcome

    Davydenko.Sergey
    Associate II
    April 18, 2015
    Posted on April 18, 2015 at 16:19

    Faced with a similar problem ...

    STM32F429 + RTOS + LWIP

    Helped.

    My thanks :)

    Half a day trying to deal with the problem ...

    Yes, I agree.

    It would be necessary in the cube to fix something for default settings LWIP + RTOS.

    Bino
    ST Employee
    April 23, 2015
    Posted on April 23, 2015 at 14:42

    You are right, in the next STM32CubeMX release, the default value of TCPIP_THREAD_STACKSIZE will be different than zero to avoid the problem you encountered.