Can this be done with a STM32F103ZE
Hello,
I have no experience at all with micro controllers & only brief experience with wiring up electronics / & some low-level programming, so please accept my apologies up-front.
I have a need to create a device that:
a. Has ONE (1) incoming RS232 port
b. Has FOUR (4) separate outgoing RS232 ports
c. ''reads'' an incoming RS232 stream,
d. look at the first 2 Bytes of info
e. check for the ''address'' (2nd byte)
f. if it is addressed ''FF 01 .........'', forward the complete original data out PORT 1 ONLY
g. if it is addressed ''FF 02 .........'' re-address the data to ''FF 01 ........'' and forward the complete data out PORT 2 ONLY
h. if it is addressed ''FF 03 .........''
re-address the data to ''FF 01 ........'' and forward the complete data out PORT 3 ONLY
i. if it is addressed ''FF 04 .........''
re-address the data to ''FF 01 ........'' and forward the complete data out PORT 4 ONLY
Here is a drawing of this for those who are more ''visual'' like me.
https://communities.intel.com/servlet/JiveServlet/showImage/2-284311-243094/PelcoD---prototype.jpg
The baud rate is 9600, 8, N, 1 (no flow control), if that helps.
Is this possible with the STM32F103ZE?
If so, would anyone be willing to ''tutor'' me in learning how to get this done?
If not, would anyone be able to suggest a more suitable platform to achieve it?
Many thanks in advance,
duBe