Skip to main content
mclapd
Associate III
October 14, 2015
Question

Way to implement both Netconn TCP server and client on same IP address

  • October 14, 2015
  • 2 replies
  • 749 views
Posted on October 14, 2015 at 02:47

Hi All,

I am now using Netconn based HTTP(web server) and TCP server on STM32F429I Eval board. HTTP and TCP server are running on each thread (FreeRTOS) and both connections are created by Neconn API,  netconn_new(NETCONN_TCP). They look working well. And I had to add TCP client so I made one more thread and tried to make connection using newconn_new(TCP) but there was system halt in vSemaphoreCreateBinary(), actually pvPortMalloc(). How can I put both TCP server and client on same IP? Any advice will be very thankful.

Regards

Chris

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    October 22, 2015
    Posted on October 22, 2015 at 12:28

    Hi Chris,

    The system halt in vSemaphoreCreateBinary() may be caused by:

    - unability to do dynamic memory allocation 

    - the space allocated is not enough

    - the memory management is not optimized

    And to answer your question ''How can I put both TCP server and client on same IP? '': both TCP server and client can be on the same IP but you shouldn’t use the same communication port (a port for server and another one for client).

    Both TCP server and client can be on the same IP but you shouldn’t use the same communication port (port for server and other for client)

    -Syrine –

    kapilsinghi123
    Associate II
    June 22, 2017
    Posted on June 22, 2017 at 20:38

    Hello All,

    I tried to run client and server in two different threads  with two different ports (server with port 80 and client with 1234)

    But the moment my client attached to the respective server on Internet my Server application stops responding !!

    I am using the net com example provided in Cube ,

    Device used is F207 and compiling code in Keil.

    Need help !