Question
ADC different behaviour on channels although same configuration
Posted on October 26, 2015 at 13:55
Hi,
I hope someone can help me. We do have some strange behaviour with our STM32F4-Discovery Boards. Currently we capture analog data on two channels. Both channels are configured equally. Despite equal configuration the ADC channels behave differently, when connecting the same signal source and measuring the input voltage. On channel 2 the voltage drops to 0.5V. This is lower bound of the preceding amplifier. When measuring on channel 0 and connecting the oscilloscope the voltage stays the same. Can someone example this strange behaviour?/* ADC3 init function */
void MX_ADC3_Init(void) { ADC_ChannelConfTypeDef sConfig; /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion) */ hadc3.Instance = ADC3; hadc3.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV8; hadc3.Init.Resolution = ADC_RESOLUTION12b; hadc3.Init.ScanConvMode = ENABLE; hadc3.Init.ContinuousConvMode = ENABLE; hadc3.Init.DiscontinuousConvMode = DISABLE; hadc3.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc3.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc3.Init.NbrOfConversion = 2; hadc3.Init.DMAContinuousRequests = ENABLE; hadc3.Init.EOCSelection = EOC_SINGLE_CONV; HAL_ADC_Init(&hadc3); /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. */ sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_144CYCLES; HAL_ADC_ConfigChannel(&hadc3, &sConfig); /**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time. */ sConfig.Channel = ADC_CHANNEL_2; sConfig.Rank = 2; HAL_ADC_ConfigChannel(&hadc3, &sConfig); }