Skip to main content
sincoon
Associate III
December 11, 2017
Question

Using internal pullups for SDIO interface

  • December 11, 2017
  • 4 replies
  • 4279 views
Posted on December 11, 2017 at 13:55

Can I use internal pull-ups for SD card connection with SDIO interface(STM32F4xx)?

#sdio #pull-up #sd-cards
This topic has been closed for replies.

4 replies

AvaTar
Senior III
December 11, 2017
Posted on December 11, 2017 at 14:25

For short connections and low clock rates, this might work.

All examples I know use external resistors, with values much lower than the internal pull-up.

The less your resistors match the line impedance, the more distortions, and the lower the possible clock frequency (and data rate).

sincoon
sincoonAuthor
Associate III
December 11, 2017
Posted on December 11, 2017 at 14:40

But, as I see, for example, Olimex dev board with stm32f407 MCU:

0690X00000609AYQAY.png

Pullup resistors have value 33k, which is not so far from internal pullup value(~30-40k - am I right?).

AvaTar
Senior III
December 11, 2017
Posted on December 11, 2017 at 15:02

Ahhh yes, correct. Probably mixed up something with I2C pull-ups.

The F4-Discovery Baseboard has 22R series resistors (before the 47k pull-up), the Mikromedia M4 10k pull-ups.

I think you don't need to restrict to STM32F4 boards for SD card example hardware.

Tesla DeLorean
Guru
December 11, 2017
Posted on December 11, 2017 at 15:11

If the leads/traces are very short. The ideal placement is at the socket, not the IC, the prototype I built for the STM32F4-DISCO used 33K at the socket, I don't recall it being reliable without them.

I'd shot for something in the 33K to 50K range

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..