Senior
September 12, 2017
Question
SPWF01S TLS connection work with Rel 3.4 and fail with 3.5
- September 12, 2017
- 1 reply
- 459 views
Posted on September 12, 2017 at 22:34
Hello,
I have two sets of NucleoF401RE+SPWF01S, on one I have
Version 3.4 SPWF01S-150410-c2e37a3
And on the other
Version 3.5 SPWF01S-160129-c5bf5ce
I run the same application that connect to AWS IOT over TLS, the 3.4 version is working fine and connected to AWS successfully, the 3.5 fail to connect.
Any idea what could be the problem?
Attached are the log of the two sessions.
Thanks,
Eyal