Skip to main content
CAPOSIENA.Philippe
Associate II
August 25, 2017
Question

PFC doesn't work on STEVAL-IHM034V2 board

  • August 25, 2017
  • 1 reply
  • 669 views
Posted on August 25, 2017 at 11:12

Hi,

i'm using the a STEVAL-IHM034V2 board for evaluation (PFC + FOC PMSM).

I imported the project in ST Workbench 4.3. Generated files and compiled with IAR is OK. Then board is programmed.

The motor starts but the PFC doesn't work. 

I verified in the file Drive parameters.h that the PFC is enabled : the following line is present

#define PFC_ENABLED /* #define PFC_ENABLED to enable the PFC */

so the PFC should be enabled.

With serial communication i get the PFC_Status = 0x10

(Id 0x4D) 

and the PFC Flags = 0x00100010

(Id 0x4E) 

which means that the AC frequency is not in the correct range. The AC Mains Frequency is read as 0 with the serial communication (Id 0x51).

The pin for AC Mains is B4 (Timer 3 channel 2)

With an oscilloscope i measured the frequency on TP7 on the board, i have a square wave with 10ms period so the signal is OK.

Thanks

Philippe

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards