Question
STM32L1 Writing on flash works or not depending on pre-initialized values
Posted on June 21, 2015 at 09:13 Hi, I experiment an issue while writing data on flash. For testing purpose, I made an app that writes several sequence of 'a' to 'z' char to flash. Each uint_32 data contains 4 chars (a-d, e-h, ...). I use : HAL_FLASH_Program(FLASH_TYPEPROGRAM_WORD, eeAddress, data); I use an array to access the data : #define EEPROM_SIZE 14 *1024 __attribute__((__section__(''.eeprom''))) uint32_t eepromZone[EEPROM_SIZE / sizeof(uint32_t)] = { value1, value2, value3 }; Everithing works fine, except for the values which are pre-initialized in the declaration. Reading the pre-initialized values is ok. Writing on those values gives odd results while reading. If I initialize value1, value2 and value3 with 0, it works : I read abcdefghijklmno after writing 'abcd' in the first uint32, 'efgh' in the second, 'ijkl' in the third and 'mno' in the fourth. If I initialize value1=0xFFFFFFFF, value2=0, value3=0, I read 0xFF FF FB FF has the first uint32, 'efgh' in the second, 'ijkl' in the third and 'mno' in the fourth after writing ''abcdefghijklmno'' If I initialize value1=0x00FFFFFF, value2=0, value3=0, I read 0x64 FF FE FF has the first uint32, 0xFFFFFFFF in the second, 'ijkl' in the third and 'mno' in the fourth after writing ''abcdefghijklmno'' If I initialize value1=0xFFFFFFFF, value2=0xFFFFFFFF, value3=0, I read 0xFFFF FB FF has the first uint32, 0xFFFFFFFF in the second, 'ijkl' in the third and 'mno' in the fourth after writing ''abcdefghijklmno'' What could happen ? What should I do to be able to pre-populated the array at flash time and modify the values after ? If needed, here's the beginning of th ld file : /* Entry Point */ ENTRY(Reset_Handler) /* Highest address of the user mode stack */ _estack = 0x2000BFFF; /* end of RAM */ /* Generate a link error if heap and stack don't fit into RAM */ _Min_Heap_Size = 0x200; /* required amount of heap */ _Min_Stack_Size = 0x400; /* required amount of stack */ /* Specify the memory areas */ MEMORY { FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 384K RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 48K } /* Define output sections */ SECTIONS { /* The startup code goes first into FLASH */ .isr_vector : { . = ALIGN(4); KEEP(*(.isr_vector)) /* Startup code */ . = ALIGN(4); } >FLASH .eeprom : { . = ALIGN(4); *(.eeprom) . = ALIGN(4); } >FLASH /* The program code and other data goes into FLASH */ .text : { . = ALIGN(4); *(.text) /* .text sections (code) */ *(.text*) /* .text* sections (code) */ *(.glue_7) /* glue arm to thumb code */ *(.glue_7t) /* glue thumb to arm code */ *(.eh_frame) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(4); _etext = .; /* define a global symbols at end of code */ } >FLASH Thanks Julien