Skip to main content
JulienD
Associate III
January 2, 2018
Solved

Nucleo F303 outputs only 2.1V on DAC

  • January 2, 2018
  • 5 replies
  • 949 views
Posted on January 02, 2018 at 19:17

Hi,

Using this nucleo board, the DAC outputs only voltage from 0 to 2.1V while VDD is 3.3v.

Where's the trick?

Thanks

Julien

#dac #nucleo-f303
This topic has been closed for replies.
Best answer by Tesla DeLorean
Posted on January 02, 2018 at 19:27

What voltage do you see when you don't connect anything to the pin?

The DAC has no current sourcing ability, perhaps you need to buffer via an op-amp?

5 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
January 2, 2018
Posted on January 02, 2018 at 19:27

What voltage do you see when you don't connect anything to the pin?

The DAC has no current sourcing ability, perhaps you need to buffer via an op-amp?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JulienD
JulienDAuthor
Associate III
January 2, 2018
Posted on January 02, 2018 at 19:42

Hi Clive,

Thanks for your answer.

Hum... When I connect nothing to the pin, the voltage is 0 - 3.3v.

I dived in the sheet, max current is 100 µA.

With my configuration it is 150µA...

0690X000006048EQAQ.jpg
T J
Senior III
January 2, 2018
Posted on January 02, 2018 at 21:50

when you adjust the R1 to say 33k, did you get the 3.3V you wanted ?  

that works out at 97uA

I am interested to see this result.