Skip to main content
Sisto Zànier
Senior
February 6, 2018
Question

timestamp'' (epoch) in ''C'' without using libraries.

  • February 6, 2018
  • 4 replies
  • 3202 views
Posted on February 06, 2018 at 19:44

For an embedded project with micro STM8,  would be very useful to me to have the mathematical formula to calculate the 'timestamp' (epoch) in 'C' without using libraries because, unlike the STM32, for this family of microcontrollers does not exist. Does anyone have any suggestions?

#timestamp
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    February 6, 2018
    Posted on February 06, 2018 at 19:59

    I have this, and an implementation for gmtime()

    https://community.st.com/0D70X000006SmDJSA0

     

    https://www.cise.ufl.edu/class/cop4600/minix/src/lib/ansi/gmtime.c

     
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    February 6, 2018
    Posted on February 06, 2018 at 20:38

    https://www.cise.ufl.edu/class/cop4600/minix/src/lib/ansi/gmtime.c

    // Keil implementation flawed/empty, this has been tested
    #define YEAR0 1900 /* the first year */
    #define EPOCH_YR 1970 /* EPOCH = Jan 1 1970 00:00:00 */
    #define SECS_DAY (24L * 60L * 60L)
    #define LEAPYEAR(year) (!((year) % 4) && (((year) % 100) || !((year) % 400)))
    #define YEARSIZE(year) (LEAPYEAR(year) ? 366 : 365)
    #define FIRSTSUNDAY(timp) (((timp)->tm_yday - (timp)->tm_wday + 420) % 7)
    #define FIRSTDAYOF(timp) (((timp)->tm_wday - (timp)->tm_yday + 420) % 7)
    // http://www.cise.ufl.edu/~cop4600/cgi-bin/lxr/http/source.cgi/lib/ansi/gmtime.c
    // https://www.cise.ufl.edu/class/cop4600/minix/src/lib/ansi/gmtime.c
    const int _ytab[2][12] = {
     { 31, 28, 31, 30, 31, 30, 31, 31, 30, 31, 30, 31 },
     { 31, 29, 31, 30, 31, 30, 31, 31, 30, 31, 30, 31 } };
    struct tm * __gmtime(const time_t *timer)
    {
     static struct tm br_time;
     struct tm *timep = &br_time;
     time_t time = *timer;
     unsigned long dayclock, dayno;
     int year = EPOCH_YR;
     dayclock = (unsigned long)time % SECS_DAY;
     dayno = (unsigned long)time / SECS_DAY;
     timep->tm_sec = dayclock % 60;
     timep->tm_min = (dayclock % 3600) / 60;
     timep->tm_hour = dayclock / 3600;
     timep->tm_wday = (dayno + 4) % 7; /* day 0 was a thursday */
    { // fold so it iterates less - sourcer32@gmail.com
     unsigned long zz = dayno / 1461; // 365+365+365+366 Breaks beyond 2100
     if (zz > 32) zz = 32; // fix 2101-2106
     year += zz * 4;
     dayno -= zz * 1461;
    }
     while (dayno >= YEARSIZE(year)) {
     dayno -= YEARSIZE(year);
     year++;
     }
     timep->tm_year = year - YEAR0;
     timep->tm_yday = dayno;
     timep->tm_mon = 0;
     while (dayno >= _ytab[LEAPYEAR(year)][timep->tm_mon]) {
     dayno -= _ytab[LEAPYEAR(year)][timep->tm_mon];
     timep->tm_mon++;
     }
     timep->tm_mday = dayno + 1;
     timep->tm_isdst = 0;
     return timep;
    }
    �?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

    I modified it so it 'ages' more gracefully, and doesn't cause execution time to creep out of control

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    henry.dick
    Associate II
    February 7, 2018
    Posted on February 07, 2018 at 23:59

    It is often included as part of the library.

    If you like to roll your own, you can easily find it on the net. I often start with clock_t and clockspersec, to yield a 32bit time_t, thus maximizing compatibility.

    Tesla DeLorean
    Guru
    February 8, 2018
    Posted on February 08, 2018 at 00:22

    >>

    It is often included as part of the library.

    That's certainly my experience, although in embedded how the clock actually ticks tends to be something punted to the user.

    I've got another library I wrote doing an emulation of Win32's SYSTEMTIME, to aid portability and cross-development.

    Testing of routines is highly recommend, especially for 2038 rollover (32-bit signed), and correct behaviour in the 1901-2099 era.

    For support beyond that significantly more rigor is required. And frankly a lot of iterative solutions have ever increasing run time, so if called frequently one needs to be particularly conscious of task dead-lines if the device is expected to function for decades.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..