Skip to main content
chy
Associate
June 21, 2015
Question

How to DIY an Air Condition Monitor and Access anywhere and anytime

  • June 21, 2015
  • 0 replies
  • 676 views
Posted on June 22, 2015 at 00:26

Function description: Utilize a wifi-microcontroller (e.g., Arduino yun, Raspbery Pi or IntoRobot Atom) to collect data from multi-sensor like temperature/humidity sensor, illumination sensor, dust sensor, and meanwhile display processed information to the OLED.

0690X00000605gkQAA.png

Components: OLED(display), DHT11(Temperature/Humidity sensor), GY30(illumination sensor), GP2Y1010AU0F(dust sensor), a USB power supply, some Dupont lines, a assembly base and an IntoRobot-Atom Wifi-DUAL-CPUs-board.

0690X00000605gpQAA.png

Process:

Step1: Connect the OLED to IntoRobot-Atom (IA). The onboard 3.3v power on IA can be used to drive the OLED. The other pin-connections are D0(DC), D1(RST), D2(SDA), and D3(SCL), where the pins in the parantheses are those on the OLED. Check whether it works by download a “Air monitor�? program from the online programming platform.

0690X00000605eaQAA.png

0690X00000603SCQAY.jpg

Step2: Connect the DHT11 sensor to IA. The onboard 5V power on IA can be used to drive the sensor. The data pin of DHT11 is connected to the D15 of IA.

0690X00000603SHQAY.jpg

Step3: Connect the GY30 to IA, with the 3.3v power supply on the IA. Because GY30 is of I2C connection, connect the SDA and SCL pins to the D8 and D9 of IA respectively.

0690X00000603MkQAI.jpg

0690X00000605guQAA.png

Step4: Connect the GP2Y1010AU0F to IA. GP2Y1010AU0F is dust sensor which can be bought easily. Power the sensor with the 3.3v supply on IntoRobot-Atom. You need to connect a 220uf capacitor and a resistor. For details, please refer to the specification. The VO pin is connected to IA’s A2, and LED is connected to IA’s D

0690X00000603SgQAI.jpg

Step5: Fix the components on the assembly base as your will.

0690X00000605gzQAA.png

Step 6: Register and login to the IntoRobot Website. Enter into the online programming tab, and fork the air condition monitor program. Compile online and download to the IA. And now, you can access your DIY air condition monitor anywhere and anytime. Enjoy!

0690X00000605h4QAA.png

See Attachements 11017

Maybe you are interested in a demo I have built:

http://www.intorobot.com/index.html#explore/5581ac692239c22c2e00000a

If you want to more technical details, please don't hesitate to contact me chy at intorobot dot com

    This topic has been closed for replies.