Skip to main content
jogerh
Associate III
June 4, 2015
Question

USART1 - interrupt problem with STM32F051

  • June 4, 2015
  • 4 replies
  • 863 views
Posted on June 04, 2015 at 17:01

Dear community,

I am trying to initialize the UART of the STM32F051 µC – however receiving of data does not work because the interrupt is not triggered. I recognized only the weak initialization of the UART1 interrupt handler in the startup file so I added myself the required lines. Unfortunately it does not work. I would be very happy if someone could check the following code for mistakes.

 

void COM_USART1_Init() { //COM_TypeDef COM, USART_InitTypeDef* USART_InitStruct)

GPIO_InitTypeDef  GPIO_InitStructure1;  //GPIO STruct

GPIO_InitTypeDef  GPIO_InitStructure2;  //GPIO STruct

USART_InitTypeDef USART_InitStructure; //USART Struct

NVIC_InitTypeDef NVIC_InitStructure;  //for USART

//GPIO for USART

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);  //GPIOA_AHBPeriph_CLOCK

 // Configure the GPIO_struct USART Tx as alternate function push-pull 

  GPIO_InitStructure1.GPIO_Pin = GPIO_Pin_9;

  GPIO_InitStructure1.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure1.GPIO_OType = GPIO_OType_PP; //PushPull (Gegentakt)

  GPIO_InitStructure1.GPIO_PuPd = GPIO_PuPd_UP; //NO Pull

  GPIO_InitStructure1.GPIO_Speed = GPIO_Speed_10MHz;

// Configure the GPIO_struct  USART Rx as alternate function push-pull 

GPIO_InitStructure2.GPIO_Pin = GPIO_Pin_10;

GPIO_InitStructure2.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure2.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure2.GPIO_PuPd = GPIO_PuPd_UP;

  GPIO_InitStructure2.GPIO_Speed = GPIO_Speed_10MHz;

  

   //Init GpioStruct

GPIO_Init(GPIOA, &GPIO_InitStructure1);

GPIO_Init(GPIOA, &GPIO_InitStructure2);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); //Connect the PINS and USART BUS

  GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);

//NVIC for USART

 USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable the USART1 receive interrupt

 USART_ITConfig(USART1, USART_IT_TXE, ENABLE); // enable the USART1 send interrupt

  // Enable the USARTx Interrupt 

  NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

 

//USART 1

 // USARTx configured as follow:

      //  - BaudRate = 115200  9600 baud  

      //  - Word Length = 8 Bits

      //  - One Stop Bit

      //  - No parity

      //  - Hardware flow control disabled (RTS and CTS signals)

      //  - Receive and transmit enabled

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);  //ENABLE USART3 CLK

   

  USART_InitStructure.USART_BaudRate = 115200;/

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

 // USART configuration 

  USART_Init(USART1, &USART_InitStructure);

    

  // Enable USART

  USART_Cmd(USART1, ENABLE);

}

void USART1_IRQHandler (void) {

if (USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) {

unsigned char received = USART_ReceiveData(USART1); //Receiver

//set DAC

}

}

//STARTUPCODE.s

USART1_IRQHandler PROC

                EXPORT  USART1_IRQHandler                [WEAK]

                B       .

                ENDP

   ; EXPORT  USART1_IRQHandler              [WEAK]

   ; EXPORT  USART1_IRQHandler              [WEAK]

Thank you very much for reviewing my code.

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    June 4, 2015
    Posted on June 04, 2015 at 17:17

    Look, you're using synchronous logic, you need to ENABLE the clock for it to function. Enable the USART1 clock *BEFORE* you touch anything inside the peripheral.

     RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);  // Do it earlier

    If you're using C++ (.CPP) watch for name mangling.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jogerh
    jogerhAuthor
    Associate III
    June 4, 2015
    Posted on June 04, 2015 at 17:59

    Thank you for responding…

    It sounds very promising however for other processors such as the STM32L100RC it seems to be not relevant since I copied and pasted the UART initialization (and just changed a few lines). Is there a significant difference between both the processor types STM32L100RC and STM32F051 regarding “synchronicity�? ? 

    Tesla DeLorean
    Guru
    June 4, 2015
    Posted on June 04, 2015 at 18:19

    They are all dependent on the correct sequencing of code, you can't just slap-dash the cut-n-paste. You need the right code, in the right order.

    void COM_USART1_Init() //COM_TypeDef COM, USART_InitTypeDef* USART_InitStruct)
    {
    GPIO_InitTypeDef GPIO_InitStructure; //GPIO STruct
    USART_InitTypeDef USART_InitStructure; //USART Struct
    NVIC_InitTypeDef NVIC_InitStructure; //for USART
    //GPIO for USART
    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9 | GPIO_Pin_10;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
    GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; //PushPull (Gegentakt)
    GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_1); //Connect the PINS and USART BUS
    GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_1);
    //NVIC for USART
    // Enable the USARTx Interrupt
    NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
    NVIC_InitStructure.NVIC_IRQChannelPriority = 0;
    NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
    NVIC_Init(&NVIC_InitStructure);
    // USART1 configured as follow:
    // - BaudRate = 115200 baud
    // - Word Length = 8 Bits
    // - One Stop Bit
    // - No parity
    // - Hardware flow control disabled (RTS and CTS signals)
    // - Receive and transmit enabled
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); //ENABLE USART1 CLK
    USART_InitStructure.USART_BaudRate = 115200;
    USART_InitStructure.USART_WordLength = USART_WordLength_8b;
    USART_InitStructure.USART_StopBits = USART_StopBits_1;
    USART_InitStructure.USART_Parity = USART_Parity_No;
    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
    USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
    // USART configuration
    USART_Init(USART1, &USART_InitStructure);
    // Enable USART
    USART_Cmd(USART1, ENABLE);
    USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); // enable the USART1 receive interrupt
    // DON'T ENABLE UNLESS YOU HAVE DATA TO SERVICE IT
    // USART_ITConfig(USART1, USART_IT_TXE, ENABLE); // enable the USART1 send interrupt
    }
    
    

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    jogerh
    jogerhAuthor
    Associate III
    June 5, 2015
    Posted on June 05, 2015 at 08:35

    Dear Clive1,

    thank you very much - now USART1 is able to receive data while triggering the interrupt.