Skip to main content
gpdonnarumma
Associate
June 15, 2018
Question

STM32L433RC Flash Memory Map

  • June 15, 2018
  • 3 replies
  • 1391 views
Posted on June 15, 2018 at 11:50

Hi, I'm working with a NUCLEO-L433RC board and I'm trying to use storage_on_flash library (

https://os.mbed.com/teams/mbed_controller/code/storage_on_flash/file/2bb58064d0a2/SOFBlock.h/

)

This library works well on the NUCLEO-F401/F411 board. Inside the file 'SOF_dev_stm32_f4xx.cpp' I can see the Flash Memory Sector Address structure.

&sharpif defined(STM32F401xE) || defined(STM32F411xE) || defined(STM32F407xx)

static const SOF_SectorSpec_t _sec_spec[] = {

{FLASH_SECTOR_0, 0x08000000, 16*1024},

{FLASH_SECTOR_1, 0x08004000, 16*1024},

{FLASH_SECTOR_2, 0x08008000, 16*1024},

{FLASH_SECTOR_3, 0x0800C000, 16*1024},

{FLASH_SECTOR_4, 0x08010000, 64*1024},

{FLASH_SECTOR_5, 0x08020000, 128*1024},

{FLASH_SECTOR_6, 0x08040000, 128*1024},

{FLASH_SECTOR_7, 0x08060000, 128*1024},

};

&sharpendif

The NucleoL433 board uses a STM32L433RC cpu that has different flash memory address.

Where I can find Flash Memory Sector Addresses for STM32L433RC

cpu?

Can someone help me?

Thank you.

#mbed #flash-storage #nucleo-l433rc #stm32
This topic has been closed for replies.

3 replies

STOne-32
ST Technical Moderator
June 15, 2018
Posted on June 15, 2018 at 14:49

Hi,

Flash Area , it’s mapping, Pages/ Sectors  on STM32F4 and STM32L4 are completely different. In F4 we have big size sectors, in L4 the sectors are small. You can find details in our Product Reference Manuals.

Cheers

STOne-32

gpdonnarumma
Associate
June 15, 2018
Posted on June 15, 2018 at 17:36

Hi,

thank you for your fast reply.

can you please show me where I can fibd this information in the datasheet?

I can only see where the flash memory begins but I can't see the different sectors address or size.

Thank you

Tesla DeLorean
Guru
June 15, 2018
Posted on June 15, 2018 at 17:41

http://www.st.com/content/ccc/resource/technical/document/datasheet/f7/a0/fc/27/24/4e/4f/3f/DM00257192.pdf/files/DM00257192.pdf/jcr:content/translations/en.DM00257192.pdf

 

3.4 Embedded Flash memory

STM32L433xx devices feature up to 256 Kbyte of embedded Flash memory available for

storing programs and data in single bank architecture. The Flash memory contains 128

pages of 2 Kbyte.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..