Skip to main content
Suthar.Narendra
Associate II
February 14, 2017
Question

STM32F429 Interface with OV5640

Posted on February 14, 2017 at 07:01

Hi,

I have interfaced OV5640 camera with STM32F429VI using DCMI and DMA. 

I am capturing JPEG image. The data of image storing in external SRAM using DMA. SRAM size is 512 x 16Bit.

I can able to store image which has size below 256KB in SRAM.

If image size increase beyond this then STM is not receiving DCMI_IT_FRAME interrupt. 

I have checked camera VSYNC, HREF and PCLK signal in this case. They are same as earlier.

Please help me to resolve this issue. 

    This topic has been closed for replies.