Skip to main content
Sebastian Juch
Associate II
September 11, 2017
Question

STM32F071RB stdperiph_lib support ?

  • September 11, 2017
  • 2 replies
  • 743 views
Posted on September 11, 2017 at 14:09

Hey,

does someone use stdperiph_lib V1.5 in combination with stm32f071rb ?

Just read in the changelog that it was updated in Dec. 2015:

  • Add support of the STM32F070xB,

    STM32F070x6 and

    STM32F030xC

      devices.

But did not find anything regarding to stm32f071rb.

Is there a solution or is the cpu only fully supported inside the HAL of CubeMx ?

Regards

Sebastian

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    September 11, 2017
    Posted on September 11, 2017 at 15:51

    And oddly the F071RB page keeps referencing the F072 part

    http://www.st.com/en/microcontrollers/stm32f071rb.html

     

    Assume it's an F072 but without CAN/USB

    Probably about time ST did a refresh on the release to cover current offerings and part numbering schemes.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Sebastian Juch
    Associate II
    September 11, 2017
    Posted on September 11, 2017 at 16:05

    Hey Clive thank you for the advice. Now i see it too, stm32f071rb and they talking about stm32f072 ... :)

    So i try using the lib with STM32F072 define and hoping that all goes right.

    What i did before is using the startup file from CubeMx and add it simply to the stdlib but i think using the define of F072 would be the better way.

    Thank You. I will report. I Hope that this will also fix the strange behavior of my DAC and ADC_DMA combination.