Skip to main content
Senior
September 13, 2017
Solved

The HAL function to read the current output status of a GPIO

  • September 13, 2017
  • 12 replies
  • 19255 views
Posted on September 13, 2017 at 08:24

If I configure one GPIO pin to output. Is there a function in HAL to read back the current output status of it?

    This topic has been closed for replies.
    Best answer by David SIORPAES
    Posted on September 13, 2017 at 18:20

    You can use HAL_GPIO_ReadPin().

    Even if the pin is set to output the IDR register will give you its current output status.

    0690X00000608E0QAI.png

    12 replies

    David SIORPAES
    David SIORPAESBest answer
    ST Employee
    September 13, 2017
    Posted on September 13, 2017 at 18:20

    You can use HAL_GPIO_ReadPin().

    Even if the pin is set to output the IDR register will give you its current output status.

    0690X00000608E0QAI.png
    hdmi87
    Associate II
    January 17, 2020

    It is not true. If a pin is configured as open-drain output and its ODR bit value is 1, it may be pulled down externally. Then its IDR bit is 0, but ODR bit still is 1. So, HAL_GPIO_ReadPin will return 0 while output state is 1.

    waclawek.jan
    Super User
    January 17, 2020

    Well spotted, @hdmi87​ , even if this is a rather old thread, it's always good to correct a mistake.

    It appears that there's no function in Cube/HAL to read GPIO_ODR, it appears that the pin-toggling function is the only one which mentions ODR at all.

    OTOH, reading back ODR has a relatively rare usage. Cube/HAL, as inevitably every "library" does, implements only a subset of possible functionality, and of course that subset is based on the "most often used" functionality. I'd leave this to simply reading the register.

    JW

    divergerAuthor
    Senior
    February 12, 2020

    Hi,

    Thanks for your attention to such an old question from me.

    Yes. Though it is wired, in a project I had to do this​. So, if I'm sure the output pin is not configured as OD, the method David proposed should work, right?

    Best​ regards.

    Diverger​

    remco2
    Visitor II
    August 19, 2022

    If you just want to read back what you wrote to the pin, you can check whether GPIOx->BSRR is GPIO_PIN_RESET or GPIO_PIN_SET.

    waclawek.jan
    Super User
    August 20, 2022

    Have you actually tried this?

    GPIOx_BSRR are write-only and read-as-zero.

    0693W00000QO7yeQAD.pngTo find out the state of output register, read, well, the output register, i.e. GPIOx_ODR.

    JW

    remco2
    Visitor II
    August 20, 2022

    I wouldn't answer a 4 year old question with a mind experiment so yes, I've tried it and it works.

    Associate II
    April 23, 2024

    "it doesn't have any advantage over reading the ODR register."

    Well, another two years... there are times when it's useful to know what was written to a pin, which might, indeed, be different than what is "visible" at the pin...this can be useful when you have something on a pin which can "return" a different state than what was written.

    I used this on an IC to do confirmation of a function that was written, as part of self-test:

    Write hi to external device

    Wait xx μs for it to perform it's internal function

    Read pin value - if it's now low, the device returns a "good" response

    OTOH, you may want to know that you've set the pin high, even if it reads low, in a case where you might be driving something like a high-gain npn transistor, or a low Vgth FET with a pull-down resistor...edge cases, but...

    Associate II
    April 23, 2024

    embedded systems can sometimes be helped by knowing the true "schematic" of the I/O pins, to allow more intimate knowledge of the behaviour in "funny" applications, or for more effective self-test operations.

    Just a thought, based on 46 years of embedded systems and IC development (about 2 billion ICs served ;) )