2016-10-11 11:37 PM
Hello,
I am working on STM32F072CB micro controller on a custom board. I am using mbed compiler and IDE for the development. I am having an issue related to the PWM pins on mcu.I have configure PB_4(pin 40) and PB_5(pin 41) pins as PwmOut pins, but I am not able to generate PWM signals on PB_5.Can you please help me to figure out issue for the same?Thank you. #mbed2016-10-12 4:15 AM
Hi saraf.akshat,
To let other community users helping you, try to provide more details about the hardware that you are using, if any external setup is established , and your code or part of it (Timer configuration for example).I recommend that you run the ready-to-use example ''TIM_PWMOutput'' in the library package at this path : STM32Cube_FW_F0_V1.6.0\Projects\STM32F072RB-Nucleo\Examples\TIM\TIM_PWMOutputTry to figure out what you have missed comparing with your own code (TIM2 is used in the example, replace it with TIM3)-Hannibal-2016-10-12 5:06 AM
Hi Hannibal,
Thanks for you response. Actually I am using mbed IDE and compiler for the development purpose. I have attached a sample PWM sample code, reference board is selected as NUCLEO-F072RB. Please check that and help me. ________________ Attachments : pwm_sample.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0rn&d=%2Fa%2F0X0000000bhQ%2FSRUeTagP_C2oMEBJ3TvhvZYYwDqc2zkbsyMSwpecfDE&asPdf=false2016-10-12 5:44 AM
And can you toggle that pin manually, if you set it as a plain output?
JW2016-10-12 6:28 AM
Hi Jan,
Yes, when i am configuring these pins as DigitalOut, these are working properly.2016-10-12 10:18 AM
Hi saraf.akshat,
I see that you have already posted in the mbed communicty for this subject. I notify our mbed developper to investigate, and I will come back to you. -Hannibal-2016-10-12 10:20 AM
According to the manual they are using PC7 (D9) for TIM3_CH2 and PB4 (D5) for TIM3_CH1
Now while I might expect getting the PWM out of PB5 (D4) TIM3_CH2 is possible, you'd likely have to dig back into the mbed pin definition stuff related to the board itself for that to happen.2016-10-12 10:07 PM
Hi Hannibal,
Thank you so much for your support.2016-10-13 2:22 AM
Hi saraf.akshat,
We confirme the bug. A pull request is greated in the Github for fixing it at thishttps://github.com/ARMmbed/mbed-os/pull/3008
Meanwhile, you can use the mbed-dev source in the mbed IDE and correct it in PeripheralPins.c as follow :replace:
  {PB_5, PWM_3, STM_PIN_DATA_EXT(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3, 1, 0)},TIM3_CH2 
by: 
{PB_5, PWM_3, STM_PIN_DATA_EXT(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3, 2, 0)}, TIM3_CH2   
  I gave you the same response on your mbed thread.
-Hannibal-2016-10-13 3:14 AM
Hi Hannibal,
Thank for the support.I have gone through the mbed library source. I found the PeripheralPins.c file, but the PWM pin definition looks like this:const PinMap PinMap_PWM[] = {// {PA_1, PWM_2, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM2)}, // TIM2_CH2 {PA_1, PWM_15, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF5_TIM15)}, // TIM15_CH1N {PA_2, PWM_15, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM15)}, // TIM15_CH1// {PA_2, PWM_2, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM2)}, // TIM2_CH3 {PA_3, PWM_15, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM15)}, // TIM15_CH2// {PA_3, PWM_2, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM2)}, // TIM2_CH4 {PA_4, PWM_14, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF4_TIM14)}, // TIM14_CH1// {PA_6, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3)}, // TIM3_CH1 {PA_6, PWM_16, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF5_TIM16)}, // TIM16_CH1// {PA_7, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3)}, // TIM3_CH2// {PA_7, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH1N// {PA_7, PWM_14, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF4_TIM14)}, // TIM14_CH1 {PA_7, PWM_17, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF5_TIM17)}, // TIM17_CH1 {PA_8, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH1 {PA_9, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH2 {PA_10, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH3 {PA_11, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH4 {PB_0, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3)}, // TIM3_CH3// {PB_0, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH2N// {PB_1, PWM_14, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM14)}, // TIM14_CH1 {PB_1, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3)}, // TIM3_CH4// {PB_1, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH3N// {PB_3, PWM_2, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM2)}, // TIM2_CH2 {PB_4, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3)}, // TIM3_CH1 {PB_5, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM3)}, // TIM3_CH2 {PB_6, PWM_16, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM16)}, // TIM16_CH1N {PB_7, PWM_17, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM17)}, // TIM17_CH1N {PB_8, PWM_16, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM16)}, // TIM16_CH1 {PB_9, PWM_17, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM17)}, // TIM17_CH1// {PB_10, PWM_2, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM2)}, // TIM2_CH3// {PB_11, PWM_2, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM2)}, // TIM2_CH4 {PB_13, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH1N {PB_14, PWM_15, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM15)}, // TIM15_CH1// {PB_14, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH2N {PB_15, PWM_15, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF1_TIM15)}, // TIM15_CH2// {PB_15, PWM_1, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF2_TIM1)}, // TIM1_CH3N// {PB_15, PWM_15, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF3_TIM15)}, // TIM15_CH1N {PC_6, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM3)}, // TIM3_CH1 {PC_7, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM3)}, // TIM3_CH2 {PC_8, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM3)}, // TIM3_CH3 {PC_9, PWM_3, STM_PIN_DATA(STM_MODE_AF_PP, GPIO_PULLUP, GPIO_AF0_TIM3)}, // TIM3_CH4 {NC, NC, 0}};I think there is no need or provision to change the Timer3 channels in definition.Should i need to look in the other source.