Skip to main content
florent239955
Associate
June 23, 2017
Question

STM32CubeMX and DHCP + UDP + NOSYS : How to configure ?

  • June 23, 2017
  • 6 replies
  • 2269 views
Posted on June 23, 2017 at 17:49

Hello,

I start a project with STM32CubeMX and a NUCLEO-F207ZG board. My goal is to have a TFTP client, but for now I'm stuck getting an IP address with DHCP. You can find my project attached.

In the lwip.c, I had to modify the MX_LWIP_Init.c file of the generated code (not in the user section), otherwise the code stops in

LWIP_ERROR('netif is not up, old style port?', netif_is_up(netif), return ERR_ARG;);

What is wrong with the STM cube configuration ?

Plus, I never go to the ethernet interrupt. How the ethernet reception is handled when there is no operating system ? (NO_SYS configuration)

Do you have a STM Cube project with DHCP and UDP (and

no TCP and no OS

) working ?

Regards,

Florent

--------

Here is a summary of my configuration in STM32CubeMx

In STM32CubeMx, I enabled LWIP. In the LWIP configuration,

-> General settings I enabled :

 - LWIP_DHCP

 - LWIP_UDP

The others are wether disabled or let to theirs default values.

-> In 'Key Options :

 - OS not used

- LWIP timer enabled

- LWIP ARP Enabled

- LWIP_NETIF_STATUS_CALLBACK Enabled

The others are wether disabled or let to theirs default values.

    This topic has been closed for replies.

    6 replies

    florent239955
    Associate
    June 26, 2017
    Posted on June 26, 2017 at 11:58

    Also, I noticed the function low_level_output in ethernetif.c return an error. I go into this ''if'' function after 4 retries from DHCP stack :

    /* Is this buffer available? If not, goto error */

          if((DmaTxDesc->Status & ETH_DMATXDESC_OWN) != (uint32_t)RESET)

          {

            errval = ERR_USE;

            goto error;

          }

    But the error is not shown as udp_sendto_if_src doesn't take the returned status into account.

    0690X00000607UHQAY.png
    florent239955
    Associate
    June 27, 2017
    Posted on June 27, 2017 at 16:09

    After setting Wireshark on the Ethernet I see the ethernet is not sending anything. I can have it working when I use the example project with tcp and freertos. But there are a lot of difference in configuration in the Ethernet register (heth).

    Also, I noticed I never enter in the following condition which start the transmission :

      /* When Tx Buffer unavailable flag is set: clear it and resume transmission */

      if (((heth->Instance)->DMASR & ETH_DMASR_TBUS) != (uint32_t)RESET)

      {

        /* Clear TBUS ETHERNET DMA flag */

        (heth->Instance)->DMASR = ETH_DMASR_TBUS;

        /* Resume DMA transmission*/

        (heth->Instance)->DMATPDR = 0U;

      }

    How the ETH_DMASR_TBUS bit is supposed to be lached ?

    I'm currently using the latest STM32CubeMX version, which is 4.21.0 with LwIP v2.0.0 (the one which comes with STMCube)

    Bino
    ST Employee
    July 5, 2017
    Posted on July 05, 2017 at 15:58

    For the first issue mentioned in

    lwip.c, it will be fixed in next STM32CubeMX release 4.22 (see

    https://community.st.com/0D50X00009Xke68SAB

    )

    florent239955
    Associate
    July 10, 2017
    Posted on July 10, 2017 at 16:03

    I finnally found the problem by comparing the STMcube project example on STM32F207ZG_NUCLEO_144. The STM cubeMX doesn't generate the proper code for the Nucleo board. First, the physical address need to be 0 instead of 1, and it only work in RMII mode.

    Stefan Hennig
    Visitor II
    August 31, 2017
    Posted on August 31, 2017 at 09:30

    That was really a helpful observation! Changing the following line in the file

    C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX\db\mcu\IP\ETH-ethermac110_v2_0_Cube_Modes.xml

    (STM32CubeMX Version 4.21.0)

    from

    <RefParameter Comment='PHY Address' DefaultValue='1' Max='31' Min='0' Name='PhyAddress' Type='integer' Group='General : Ethernet Configuration'/>

    to

    <RefParameter Comment='PHY Address' DefaultValue='0' Max='31' Min='0' Name='PhyAddress' Type='integer' Group='General : Ethernet Configuration'/>

    fixed my CubeMX installation so that I can have my NUCLEO_F207ZG talk to the Ethernet.

    It is merely a hack, I have no understanding of the inner workings of CubeMX and I don't know what else this change might break, but as the 207 is the only Ethernet-enabled target I'm working with, I can say: 'Works for me'.

    Maybe someone from STM should have a deeper look into this.