Question
link Bootloader to application starts
Posted on June 17, 2015 at 10:07
hej ,
i would like to know that, how to link JumpToApplication() to my original code starts?..can anyone guide me about this?i have written the code like the below in GCC linker file. GCC Linker file:--------------------------------------------------------MEMORY{ BOOT (rx) : ORIGIN = 0x08000000, LENGTH = 0x0000C000 rom (rx) : ORIGIN = 0x0800C000, LENGTH = 0x000F4000 ram (rwx) : ORIGIN = 0x20000000, LENGTH = 0x00020000 ram1 (rwx) : ORIGIN = 0x10000000, LENGTH = 0x00010000}_eram = 0x20000000 + 0x00020000;SECTIONS{ .boot : { KEEP(*(.isr_vector)) startup_stm32f4??.o(.text) } >BOOT-----------------------------------------------------------In the main, i have written like the below int main(void){ typedef void (*pFunction)(void); pFunction JumpToApplication; RCC_DeInit(); SysTick->CTRL = 0; SysTick->LOAD = 0; SysTick->VAL = 0; __set_PRIMASK(1); // Disable interrupts // in the core_cmFunc.h __set_MSP(*(__IO uint32_t*) APPLICATION_ADDR); // in the core_cmFunc.h jumpAddress = *(__IO uint32_t*) (APPLICATION_ADDR); JumpToApplication = (pFunction) jumpAddress; JumpToApplication();}-------thank you