Question
DMA FIFO level
Posted on March 09, 2015 at 08:39
Please, confirm
my assumption: it is typing error in RM0090? Register DMA_SxFCR STM32F4xx
Bits 1:0 FTH[1:0]: FIFO threshold selection
These bits are set and cleared by software.
00: 1/4 full FIFO
01: 1/2 full FIFO
10: 3/4 full FIFO
11: full FIFO
These bits are not used in the direct mode when the DMIS value is zero.
These bits are protected and can be written only if EN is ‘1’
Must be EN = 0?P.S.
On this forum
, it is impossible to format the message
.
This is the worst
that
can be found
.
Developer
Wake up!