Skip to main content
gl2
Associate III
Jul 1, 2015 10:14 AM UTC
Solved

[Solved] How can I print an Integer

Posted on July 01, 2015 at 12:14

Hello.

I use the board SPC560P-DISP. How can I print an Integer with Tera Term through a serial connection? I use the function chnWriteTimeout to print a string. So:

chnWriteTimeout(&SD1, (uint8_t *)
''Hello World!\r\n''
, 14, TIME_INFINITE);

But an Integer? I tried to use chprintf, but not working. It does not recognize the function chprintf. I included the header chprintf.h

uint32_t number=25;
chprintf(&SD1, 
''%u \n\r''
, number);

The error is:

main.c:(.text_vle.main+0x10c): undefined reference to `chprintf'
collect2: ld returned 1 exit status
make: *** [build/
out
.elf] Error 1

In the demo of SPC5 Studio for my board they use only chnWriteTimeout. Best regards Gianluca.
    This topic has been closed for replies.
    gl2
    gl2Best answer
    Associate III
    Jul 7, 2015 9:59 AM UTC
    Posted on July 07, 2015 at 11:59

    Ok, I solved so:

    chprintf((BaseSequentialStream *)&SD1, ''Value of dur is: %d'', dur);

    There was no cast. Thanks. Best regards Gianluca.

    3 replies

    Erwan YVIN
    ST Technical Moderator
    Jul 2, 2015 7:59 AM UTC
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    gl2
    gl2Author
    Associate III
    Jul 7, 2015 9:41 AM UTC
    Posted on July 07, 2015 at 11:41

    Hello,

    I use this code, but nothing happens. I enabled the serial connection and set the baud to 38400 of Tera Term. When I try to use chprintf nothing appears on the screen.

    /*
    ChibiOS/RT - Copyright (C) 2006-2014 Giovanni Di Sirio
    Licensed under the Apache License, Version 2.0 (the ''License'');
    you may not use this file except in compliance with the License.
    You may obtain a copy of the License at
    http://www.apache.org/licenses/LICENSE-2.0
    Unless required by applicable law or agreed to in writing, software
    distributed under the License is distributed on an ''AS IS'' BASIS,
    WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
    See the License for the specific language governing permissions and
    limitations under the License.
    */
    /* Inclusion of the main header files of all the imported components in the
    order specified in the application wizard. The file is generated
    automatically.*/
    #include ''components.h''
    #include ''shellcmd.h''
    /*
    * Shell configuration structure, the first field is the serial port used by
    * the shell, the second is the array of commands accepted by the shell and
    * defined in shellcmd.c.
    */
    static
    const
    ShellConfig shell_cfg1 = {(BaseSequentialStream *)&SD1,
    shell_commands};
    /*
    * LEDs blinker thread, times are in milliseconds.
    */
    static
    WORKING_AREA(waThread1, 128);
    static
    msg_t Thread1(
    void
    *arg) {
    (
    void
    )arg;
    chRegSetThreadName(
    ''blinker''
    );
    while
    (TRUE) {
    //uint32_t duration=3, distanceCm;
    unsigned 
    int
    dur=3;
    palClearPad(PORT_A, TRIG_PIN); 
    // low
    osalThreadSleepMicroseconds(2);
    palSetPad(PORT_A, TRIG_PIN); 
    //high
    osalThreadSleepMicroseconds(10);
    palClearPad(PORT_A, TRIG_PIN); 
    // low
    palTogglePad(PORT_A,Led_D12);
    //chnWriteTimeout(&SD1, (uint8_t *)''%u
    
    '', 14, TIME_INFINITE);
    chprintf(
    ''%u''
    , dur);
    osalThreadSleepMilliseconds(500);
    }
    return
    0;
    }
    /*
    * Application entry point.
    */
    int
    main(
    void
    ) {
    //Thread *shelltp = NULL;
    /* Initialization of all the imported components in the order specified in
    the application wizard. The function is generated automatically.*/
    componentsInit();
    /*
    * Activates the serial driver 1 using the driver default configuration.
    */
    sdStart(&SD1, NULL);
    /*
    * Creates the blinker thread.
    */
    chThdCreateStatic(waThread1, 
    sizeof
    (waThread1), NORMALPRIO, Thread1, NULL);
    /* Application main loop.*/
    // while (1) {
    // if (!shelltp)
    // shelltp = shellCreate(&shell_cfg1, SHELL_WA_SIZE, NORMALPRIO);
    //else if (chThdTerminated(shelltp)) {
    //chThdRelease(shelltp); /* Recovers memory of the previous shell. */
    //shelltp = NULL; /* Triggers spawning of a new shell. */
    //}
    chThdSleepMilliseconds(1000);
    //}
    }

    Why? Best regards Gianluca.
    gl2
    gl2AuthorBest answer
    Associate III
    Jul 7, 2015 9:59 AM UTC
    Posted on July 07, 2015 at 11:59

    Ok, I solved so:

    chprintf((BaseSequentialStream *)&SD1, ''Value of dur is: %d'', dur);

    There was no cast. Thanks. Best regards Gianluca.