Skip to main content
Mike Kay
Associate
October 21, 2017
Question

Communication problem between two 868 MHz sub-GHz modules

  • October 21, 2017
  • 0 replies
  • 562 views
Posted on October 21, 2017 at 17:34

Hello Everyone,

I'm struggling to setup communications between two 868 MHz sub-GHz modules.

The first module is the STEVAL-IDS001V4M (USB dongle with SPSGRF-868) and the second module is the STEVAL-SP1ML868 (USB dongle with SP1ML-868).

I'm using the Windows application 'SPIRIT1 DK Application v2.2.1' to configure the radio and packet settings of the STEVAL-IDS001V4M module, then using the 'Transmission Test' window to send the text 'Hello World'.

The radio and packet settings for the STEVAL-IDS001V4M are as follows (configured via the GUI):

Frequency Base: 867.999967 MHz

Data Rate: 38.433 kbps

Frequency Deviation: 19.836 kHz

Channel Filter: 102.115 kHz

Modulation: 2-FSK

Output Power: 0 dBm

Packet Format: BASIC

Preamble Length: 4

Sync Length: 4

Sync Value: 0x88888888

CRC: No CRC

FEC: Disabled

Data Whitening: Enabled

The radio and packet settings for the STEVAL-SP1ML868 are as follows:

S00:BAUD_RATE=115200

S01:FREQUENCY=868000000

S02:DATA_RATE=38400

S03:MODULATION=0

S04:OUTPUT_POWER=11.6

S05:FREQ_DEVIATION=20

S06:RX_FILTER=100

S07:CS_MODE=0

S08:RSSI_THRESHOLD=-130

S09:PREAMBLE_LEN=4

S10:SYNC_LENGTH=4

S11:SYNC_VALUE=0x88888888

S12:CRC_MODE=0

S13:WHITENING=1

S14:FEC=0

S15:SOURCE_ADDR=0x00

S16:DESTINATION_ADDR=0xff

S17:MULTICAST_ADDR=0xee

S18:BROADCAST_ADDR=0xff

S19:FILTER_CRC=0

S20:FILTER_SOURCE=0

S21:FILTER_DESTINATION=0

S22:FILTER_MULTICAST=0

S23:FILTER_BROADCAST=0

S24:TX_RX_LED=1

S25:RESERVED=

S26:ESCAPE_SEQ=1

S27:SOURCE_FILT_MASK=0x00

S28:PAYLOAD_SIZE=32

The data received from the STEVAL-SP1ML868 is:

ccy»{c#

Something is being received but not 'Hello World'.

I assume the two dongles are compatible? They both use the SPIRIT1 module.

I'd be very grateful if anyone can help or provide any suggestions.

Mike.

This topic has been closed for replies.